To build and run the IPCF Sample program (S32 IPCF 1.1.0 D2012) on S32DS (Ver: 3.3,Build id: 2006)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

To build and run the IPCF Sample program (S32 IPCF 1.1.0 D2012) on S32DS (Ver: 3.3,Build id: 2006)

8,814 Views
_manoj_kumar
NXP Employee
NXP Employee

Hello Team,

Customer facing below errors in S32 DS 3.3, pls advice:

    • Error: Processor 'S32G274A' detected in Design Studio GCC project does not match with currently selected `S32G274A_Rev2`.
    • Level: Error
    • Type: Tool problem
    • Tool: McuConfiguration
    • Origin: IPCF_Example_S32G274
    • Resource: Processor
    • Information: -
  • If they switch to S32G274A, then there are attached build errors

Please find more details.

Design Studio : Version: 3.3,Build id: 200610

RTD Version : SW32G2_RTD_4.4_0.9.0

IPCF Sample program (S32 IPCF 1.1.0 D2012

Documents Referred: IPCF Shared Memory Driver User Manual Version 1.4

They are observing issues in S32 Design Studio. They are unable to select appropriate hardware to configure.

Once the IPCF example project is imported in DS, there is a mismatch BGA observed.

_manoj_kumar_0-1614594447759.jpeg

Even if they choose S32G2745A_525bga the tool does not support selected processor.

_manoj_kumar_1-1614594447728.jpeg

Please let me know if you need any other details to be checked with them

Thanks

0 Kudos
Reply
4 Replies

8,755 Views
mikedoidge
NXP Employee
NXP Employee

Hello @_manoj_kumar ,

It's possible some package or update is not installed. Could you please go to S32DS Extensions and Updates menu and click on 'Installation Details' link at upper right. Then send the details of the installed packages.

mikedoidge_0-1615501520413.png

 

Thanks,

Mike

0 Kudos
Reply

8,729 Views
_manoj_kumar
NXP Employee
NXP Employee

Hello Mr. Mike,

The solution for this issue was provided. Please find the link below.

https://community.nxp.com/t5/Vehicle-Control-and-Networking/To-build-and-run-the-IPCF-Sample-program...

Thanks.

8,806 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please attach pictures with higher resolution. Attached ones are too small and unreadable. Thanks. 

 

Jiri 

0 Kudos
Reply

8,790 Views
_manoj_kumar
NXP Employee
NXP Employee

Hi,

I have attached the error snapshots. Please let me know if you need any other details.

Thanks.

0 Kudos
Reply