Symbol viewer in Design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Symbol viewer in Design studio

ソリューションへジャンプ
2,187件の閲覧回数
Catosh
Contributor IV

Hi All, 

on MCUXpresso there is the symbol viewer but I can't find it on S32 Design Studio. Is it there, hidden somewhere? or do I need to enable it somewhere in the eclipse preferences?

Thanks and best regards, 

L.

P.S.

Erich Styger on his MCU on Ecliupse provides many alternatives if not, from AMAP to the nm option:

arm-none-eabi-nm -S --size-sort -s MyBinary.axf

0 件の賞賛
返信
1 解決策
2,095件の閲覧回数
BlackNight
NXP Employee
NXP Employee

That Symbol viewer is specific for the MCUXpresso IDE (see Listing Code and Data Size with GNU nm in Eclipse | MCU on Eclipse)  and is not available in the S32 Design Studio.

Erich

元の投稿で解決策を見る

1 返信
2,096件の閲覧回数
BlackNight
NXP Employee
NXP Employee

That Symbol viewer is specific for the MCUXpresso IDE (see Listing Code and Data Size with GNU nm in Eclipse | MCU on Eclipse)  and is not available in the S32 Design Studio.

Erich