Symbol viewer in Design studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Symbol viewer in Design studio

Jump to solution
2,170 Views
Catosh
Contributor IV

Hi All, 

on MCUXpresso there is the symbol viewer but I can't find it on S32 Design Studio. Is it there, hidden somewhere? or do I need to enable it somewhere in the eclipse preferences?

Thanks and best regards, 

L.

P.S.

Erich Styger on his MCU on Ecliupse provides many alternatives if not, from AMAP to the nm option:

arm-none-eabi-nm -S --size-sort -s MyBinary.axf

0 Kudos
Reply
1 Solution
2,078 Views
BlackNight
NXP Employee
NXP Employee

That Symbol viewer is specific for the MCUXpresso IDE (see Listing Code and Data Size with GNU nm in Eclipse | MCU on Eclipse)  and is not available in the S32 Design Studio.

Erich

View solution in original post

1 Reply
2,079 Views
BlackNight
NXP Employee
NXP Employee

That Symbol viewer is specific for the MCUXpresso IDE (see Listing Code and Data Size with GNU nm in Eclipse | MCU on Eclipse)  and is not available in the S32 Design Studio.

Erich