SPT Kernel programming S32R274

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPT Kernel programming S32R274

1,693 次查看
User133
Contributor II

Hi, 

I have a couple questions I would really appreciate an answer to. 

1. I want to program my own kernel for S32R274 for Radar detection. Where can I do this? I have downloaded S32 Design Studio Power Architecture. 

1a. what does it mean that the kernels can be programmed on MATLAB? Does this mean they can simulated on MATLAB, since obviously the board does not work directly with MATLAB. (I did download the toolbox) 

2. Where can I configure the middleware of the board, so that it may perform certain functions. Is this main? I am asking because the demo file did not work on my board. 

Thank you in advance 

0 项奖励
回复
1 回复

1,684 次查看
mikedoidge
NXP Employee
NXP Employee

Hello,

Yes, MATLAB is used for simulation, not actual HW. I recommend you to check out the community for this:  MBDT for RADAR - NXP Community  

Make sure to install the RSDK 1.5.0 for S32R274 and S32R372.  It contains example projects for you to try. Unfortunately, there is no community for the RSDK, you will need to submit a support ticket to Support | NXP Semiconductors if you have issues with the RSDK examples.

Mike

0 项奖励
回复