SPT Kernel programming S32R274

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPT Kernel programming S32R274

1,703 Views
User133
Contributor II

Hi, 

I have a couple questions I would really appreciate an answer to. 

1. I want to program my own kernel for S32R274 for Radar detection. Where can I do this? I have downloaded S32 Design Studio Power Architecture. 

1a. what does it mean that the kernels can be programmed on MATLAB? Does this mean they can simulated on MATLAB, since obviously the board does not work directly with MATLAB. (I did download the toolbox) 

2. Where can I configure the middleware of the board, so that it may perform certain functions. Is this main? I am asking because the demo file did not work on my board. 

Thank you in advance 

0 Kudos
Reply
1 Reply

1,694 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

Yes, MATLAB is used for simulation, not actual HW. I recommend you to check out the community for this:  MBDT for RADAR - NXP Community  

Make sure to install the RSDK 1.5.0 for S32R274 and S32R372.  It contains example projects for you to try. Unfortunately, there is no community for the RSDK, you will need to submit a support ticket to Support | NXP Semiconductors if you have issues with the RSDK examples.

Mike

0 Kudos
Reply