S32ds studio version 3.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32ds studio version 3.4

1,060件の閲覧回数
Anjalipurushothaman
Contributor III

will the S32ds studio version 3.4 support family S32K388 OR S32K358?

0 件の賞賛
返信
1 返信

1,045件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

From the Release Notes of the RTD of S32K358 and S32K388, it can be seen that it is developed based on S32 Design Studio 3.5. So if you need to develop S32K358\S32K388 , please use S32DS v3.5 instead of v3.4.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信