S32K3xx RTD Installation Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3xx RTD Installation Issue

Jump to solution
5,108 Views
Vignesh_S
Contributor III

Hi,

We are using the S32K3X4EVB-T172 Evaluation Board and We are trying to load the example file in the EVK board..

I installed S32 Design studio 3.5, S32K3xx development package (SW32K3xx_S32DS_3.5.0_D2303.zip).

After that I tried to install the RTD files(SW32K3_RTD_4.4_R21-11_3.0.0_D2303_DS_updatesite.zip) But im facing the below issue.

 
 

Operation details Software being installed: com.nxp.RTD.S32K3XX.root.feature.feature.group 3.0.0.202303311831 Missing requirement: com.nxp.RTD.S32K3XX.root.feature.feature.group 3.0.0.202303311831 requires 'org.eclipse.equinox.p2.iu; com.nxp.s32ds.platform.ide.feature.feature.group 3.5.1' but it could not be found

 

After the S32K3xx development package installation im able to create a new project for S32K344 but im unable to open any example files. 

Please help me to solve this issue.

 

0 Kudos
Reply
1 Solution
5,002 Views
Vignesh_S
Contributor III

Thanks. Issue is resolved after installing the correct development package.

View solution in original post

0 Kudos
Reply
2 Replies
5,061 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please make sure that you updated S32 Design Studio Platform Package and S32 Design Studion Platform Tools Package to latest vesion:

jiri_kral_0-1684762432935.pngjiri_kral_0-1684762432935.png

 

5,003 Views
Vignesh_S
Contributor III

Thanks. Issue is resolved after installing the correct development package.

0 Kudos
Reply