S32K344 debugging with Segger J Link and S32DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K344 debugging with Segger J Link and S32DS

7,214 次查看
swcoder
Contributor I

Hi,

I have a S32K3X4EVB-Q257 evaluation board and have installed S32DS 3.4(Update 3) IDE.

Segger J link version is 7.60f.

I am trying to debug the Digital IO Led toggle example on the board through the IDE with Segger J link.

However I get the following error on debug window. I am not able to see the disassembly or place breakpoints.

swcoder_0-1643812011148.png

My settings for debug are:

swcoder_1-1643812446902.png

 

swcoder_2-1643812480857.png

Debug output console:

swcoder_3-1643812988776.png

Can anyone please guide me on this.

Thanks

标记 (4)
0 项奖励
回复
7 回复数

7,162 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

I can reproduce your issue. On my side - sometimes - especially with very first debug session - it works normally. But next debug session fails in the very same way like on your pictures. With PE Micro it works normally. 

 

I didn't find the reason, it is probably something with Segger plugin - you can ask on Segger's forum. 

 

Jiri

0 项奖励
回复

7,055 次查看
tsirkunenkoa
Contributor II

What if using a PE Micro debugger is not an option? We have to use the J-Link debuggers in our project.

I just don't understand how come we are not able to use a basic example project for the board that is meant to be used with the J-Link debuggers apart from PE Micro ones?

0 项奖励
回复

7,142 次查看
swcoder
Contributor I

Does it work with the on board debugger with micro USB cabel?

Can you verify that once please?

Or does it give the same issue?

0 项奖励
回复

7,125 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

yes, debugging works with Integrated PE micro debugger or wot external PE Micro debug probe. 

 

Jiri

0 项奖励
回复

6,962 次查看
MateoSegura413
Contributor III

Lots of issues with the SEGEGR debugger. FreeRTOS will not go past the SVC instruction to start the first task. Please please please get someone at NXP to test this and debug it, it is crucial for any project that's not using an eval kit

0 项奖励
回复

5,656 次查看
timwhite
Contributor III

I feel your pain.

0 项奖励
回复

6,795 次查看
xuchaochen
Contributor I

you need to use hard reset when using SEGEGR debugger. when just using soft reset, there are some regs not be reset.

0 项奖励
回复