S32K312 STM clock issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K312 STM clock issues

ソリューションへジャンプ
15,162件の閲覧回数
JayJay_H
Contributor III

Hi

Recently, I have been using STM0 as a millisecond level timestamp to start timing from power on

Prescaler is 240,clock source is FIRC_CLK(48Mhz)

The time is obtained through the Stm_Ip_GetCounterValue(0) interface

During use, it was found that the obtained time was faster than normal time, for example, the actual time passed 500ms but the obtained time was 600ms, and it has been getting faster all the time

But when I switch the clock source to AIPS_PLAT_CLK(60MHz) or FXOSC_CLK(16MHz), the time value obtained from the interface is accurate

The attached image shows my configuration of STM and Clock in DS. Do I have any other options to configure?

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
14,933件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @JayJay_H,

It means TS1_CLK is clocked from AIPS_PLAT_CLK.

If you have any question on Time stamps, please create a new thread.

 

Thank you,

BR, Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
15,134件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @JayJay_H,

I can't explain the 20% inaccuracy.

But +-5% can be expected.

danielmartynek_1-1707228376518.png

 

FIRC can be measured at CLKOUT.

S32K312 clock system diagram

danielmartynek_0-1707228263324.png

 

Regards,

Daniel

 

0 件の賞賛
返信
15,126件の閲覧回数
JayJay_H
Contributor III

Hi Daniel

Thank you for your reply

What about AIPS_PLAT_CLK and FXOSC_CLK

Is there any inaccuracy in AIPS_PLAT_CLK and FXOSC_CLK?

If so, what is the inaccuracy range,also +-5%?

Best regards,

Jay

0 件の賞賛
返信
15,119件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jay,

The accuracy of FXOSC is given by the tolerance of the external crystal/resonator.

If AIPS_PLAT_CLK is generated by the SPLL, there is Jitter specified in the DS, Table 41.

 

Regards,

Daniel

 

 

 

 

 

Best regards,

Daniel

 

 

 

0 件の賞賛
返信
15,006件の閲覧回数
JayJay_H
Contributor III

Hi Daniel

Thanks for your reply.

I found the following attachment while reading  the referance manual

My questions are:

what's the meaning of "TS1_CLK—AIPS_PLAT_CLK" ?

According to the attachment,  does it means that STM0 should use AIPS_PLAT_CLK?

 

(Please forgive me for replying to you so late, recently it was Chinese New Year and I was on holiday

BTW, Happy New Year of the Loong)

0 件の賞賛
返信
14,934件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @JayJay_H,

It means TS1_CLK is clocked from AIPS_PLAT_CLK.

If you have any question on Time stamps, please create a new thread.

 

Thank you,

BR, Daniel

0 件の賞賛
返信