S32K148 clock configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K148 clock configuration

3,390件の閲覧回数
347996379
Contributor III

In SDK development kit, the clock configuration of S32K148 is 8M external crystal oscillator. Can it support 16M crystal oscillator?8M external crystal oscillator is recommended or must be 8M external crystal oscillator?

タグ(3)
0 件の賞賛
返信
5 返答(返信)

3,236件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Examples are part of S32DS Installation. Just click on File -> New -> Project from Example and choose one which you are interested in: 

pastedImage_1.png

pastedImage_2.png

Jiri 

0 件の賞賛
返信

3,236件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi,

for S32K148 you can use external oscillator from 4 to 40 MHz. There are two modes used in SDK for system OSC range select - medium for 4-8 MHz crystals and high for 8-40MHz crystals:

pastedImage_1.png

Jiri 

0 件の賞賛
返信

3,236件の閲覧回数
347996379
Contributor III

Thank you for your reply!It's too much trouble to delete things I don't need myself in your SDK,so I want to create my own SDK. Do you have any tutorials?

0 件の賞賛
返信

3,236件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

actually - there is no such tutorial. There is couple non-SDK examples for S32K144, you can modify them and use with S32K148.

Jiri

0 件の賞賛
返信

3,236件の閲覧回数
347996379
Contributor III

Can you give it to me?

0 件の賞賛
返信