S32K DS update problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K DS update problem

Jump to solution
12,843 Views
Zyuan17
Contributor III

I am trying to update my S32K DS, but the pop-up window shows that there is an error happened during the update. It says an error occurred while collecting items to be installed.

 

The details:

An error occurred while collecting items to be installed
session context was:(profile=SDKProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: osgi.bundle,com.pemicro.core,1.3.4
No repository found containing: osgi.bundle,com.pemicro.debug.gdbjtag.pne,5.2.6.202206301831
No repository found containing: org.eclipse.update.feature,com.pemicro.debug.gdbjtag.pne.feature,5.2.6.202206301831

0 Kudos
Reply
1 Solution
12,701 Views
mikedoidge
NXP Employee
NXP Employee
0 Kudos
Reply
7 Replies
12,798 Views
m_mishrikey
Contributor III

Me too with 3.5.  Here is the error dialog.

The addresses it is trying to access don't work if I type them into URL of web browser.

m_mishrikey_0-1665158271885.pngm_mishrikey_0-1665158271885.png

 

0 Kudos
Reply
12,820 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

 

I'm not sure what is your S32DS version - you can try to update PE Micro driver first - https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Install-update-from-3rd-party-ve...

 

0 Kudos
Reply
12,819 Views
Zyuan17
Contributor III

It's still not working. The pop-up window shows the same problem.

 

An error occurred while collecting items to be installed
session context was:(profile=SDKProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: osgi.bundle,com.pemicro.debug.gdbjtag.ppc,2.0.4.202103012147
No repository found containing: org.eclipse.update.feature,com.pemicro.debug.gdbjtag.ppc.feature,2.0.4.202103012147

0 Kudos
Reply
12,835 Views
Prem_Venkata_Subbarao
Contributor II
I am also facing the same issue.
0 Kudos
Reply
12,709 Views
mikedoidge
NXP Employee
NXP Employee

Hello @Prem_Venkata_Subbarao@Zyuan17@m_mishrikey,

Please share the installation details of your S32 Design Studio installation configuration.

1) Help -> S32DS Extensions and Updates

2) Click 'Installation Details'

image.pngimage.png

3) Copy the text and share it to this thread.

Thanks,

Mike

0 Kudos
Reply
12,704 Views
m_mishrikey
Contributor III

Package: GDB Client for ARM Embedded Processors 9.2 Build 1701; Version: 1701; Build id: 202012011653

Package: S32 Design Studio Platform package; Version: 3.5.0; Build id: 202207261752

Package: GNU ARM PEMicro Interface Debugging Support; Version: 5.1.7; Build id: 202112141853

Package: S32 Design Studio Platform Tools package; Version: 3.5.0; Build id: 202207261752

Package: NXP GCC for Arm Embedded Processors Build 1620; Version: 1620; Build id: 202005201521

0 Kudos
Reply
12,702 Views
mikedoidge
NXP Employee
NXP Employee

Ok, just realized this is the same issue we are discussing on the other thread: https://community.nxp.com/t5/S32-Design-Studio/Extensions-and-Updates-not-working-correctly/m-p/1540...

 

0 Kudos
Reply