S32G RTD errors in S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G RTD errors in S32DS

Jump to solution
7,737 Views
Rick_Li
NXP Employee
NXP Employee

Hello there,

I got some errors when created an S32G RTD configuration project in S32DS.

these errors show that peripherals drivers are not found in toolchain/IDE project.

see attached image.

any suggestion?

Many thanks.

Labels (1)
0 Kudos
Reply
1 Solution
7,724 Views
Rick_Li
NXP Employee
NXP Employee

the problem solved.

right click error and then "add ..." will solve the issue.

View solution in original post

4 Replies
7,025 Views
murphy_xie
Contributor I

Hi nxp

     when I trying to install RTD as  S32 Design Studio v3.4.1及RTD 2.0.0 HF4安装指南_v20210810.pdf 

,but I can not find RTD package for S32G2,only S32K1 and S32k3 valueable,can you help to solve it,tks.
0 Kudos
Reply
7,020 Views
Rick_Li
NXP Employee
NXP Employee
0 Kudos
Reply
7,007 Views
murphy_xie
Contributor I

Hi Rick

   tks,it working.

B.R

 

0 Kudos
Reply
7,725 Views
Rick_Li
NXP Employee
NXP Employee

the problem solved.

right click error and then "add ..." will solve the issue.