CCS to scan JTAG for S32R45

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CCS to scan JTAG for S32R45

1,560 Views
PraveenKumar_K
Contributor II

Hi Team,

I am using S32 Debug probe with S32R EVK, I use the CCS.exe to check the S32 probe can connect to S32R CPU or not from CCS console window. 

below is the image, when I tried to check it.

CCS_server.PNG

  

 

"JTAG DAP ID is invalid". can anyone give me some suggestion on how to solve this S32 Debug Probe issue.

 

Thanks in advance..

 

Labels (2)
0 Kudos
Reply
3 Replies

1,549 Views
mikedoidge
NXP Employee
NXP Employee

Hello Praveen,

This script will be deprecated in future release. It has already been replaced by the 'Test Connection' buttion in the Debug Configurations menu. It was not maintained so it reports this invalid state. It is not a symptom of any other issue.

Best Regards,

Mike

1,539 Views
PraveenKumar_K
Contributor II

Thanks for your reply. I used to check the 'Test Connection' button. It shows "The Board is Connected". But still I am not able to debug the with the probe, so I tried with that method to check the JTAG scanning.

 

Thanks.

0 Kudos
Reply

1,471 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

Sorry for the long delay, is your EVB setup to boot from Linux BSP? If so, please change the setup so it does not boot Linux OS. If Linux BSP is running when S32 Debugger is trying to connect via JTAG, it could be interrupted. The S32 Debugger does not yet have Linux-aware debugging enabled.

Best Regards,

Mike

0 Kudos
Reply