S32G RTD errors in S32DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32G RTD errors in S32DS

跳至解决方案
5,550 次查看
Rick_Li
NXP Employee
NXP Employee

Hello there,

I got some errors when created an S32G RTD configuration project in S32DS.

these errors show that peripherals drivers are not found in toolchain/IDE project.

see attached image.

any suggestion?

Many thanks.

标签 (1)
0 项奖励
回复
1 解答
5,537 次查看
Rick_Li
NXP Employee
NXP Employee

the problem solved.

right click error and then "add ..." will solve the issue.

在原帖中查看解决方案

4 回复数
4,838 次查看
murphy_xie
Contributor I

Hi nxp

     when I trying to install RTD as  S32 Design Studio v3.4.1及RTD 2.0.0 HF4安装指南_v20210810.pdf 

,but I can not find RTD package for S32G2,only S32K1 and S32k3 valueable,can you help to solve it,tks.
0 项奖励
回复
4,833 次查看
Rick_Li
NXP Employee
NXP Employee
0 项奖励
回复
4,820 次查看
murphy_xie
Contributor I

Hi Rick

   tks,it working.

B.R

 

0 项奖励
回复
5,538 次查看
Rick_Li
NXP Employee
NXP Employee

the problem solved.

right click error and then "add ..." will solve the issue.