S32DS3.4 debug configuration Ram Application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS3.4 debug configuration Ram Application

跳至解决方案
2,394 次查看
tianxing
Contributor IV

tianxing_0-1639466875113.png

What does the Ram application mean?

If not select Ram application S32DS cannot debug and always has the warrning that Failed to read memory @ address 0x20020000

 

 

0 项奖励
回复
1 解答
2,373 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

if you are using RAM target application - (instead of FLASH target) after reset your binary disappears from RAM. With this option enabled - after reset is your binary again upload into RAM. 

 

Jiri 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,374 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

if you are using RAM target application - (instead of FLASH target) after reset your binary disappears from RAM. With this option enabled - after reset is your binary again upload into RAM. 

 

Jiri 

0 项奖励
回复
2,361 次查看
tianxing
Contributor IV

Hi

I am using Flash target application. What's the difference between with Ram Application and without Ram Application?

0 项奖励
回复
2,348 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

This option is ignored for Flash target application. 

 

Jiri

0 项奖励
回复