S32DS3.4 debug configuration Ram Application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.4 debug configuration Ram Application

Jump to solution
3,382 Views
tianxing
Contributor IV

tianxing_0-1639466875113.png

What does the Ram application mean?

If not select Ram application S32DS cannot debug and always has the warrning that Failed to read memory @ address 0x20020000

 

 

0 Kudos
Reply
1 Solution
3,361 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

if you are using RAM target application - (instead of FLASH target) after reset your binary disappears from RAM. With this option enabled - after reset is your binary again upload into RAM. 

 

Jiri 

View solution in original post

0 Kudos
Reply
3 Replies
3,362 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

if you are using RAM target application - (instead of FLASH target) after reset your binary disappears from RAM. With this option enabled - after reset is your binary again upload into RAM. 

 

Jiri 

0 Kudos
Reply
3,349 Views
tianxing
Contributor IV

Hi

I am using Flash target application. What's the difference between with Ram Application and without Ram Application?

0 Kudos
Reply
3,336 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

This option is ignored for Flash target application. 

 

Jiri

0 Kudos
Reply