S32DS for ARM 2018R1 license

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS for ARM 2018R1 license

Jump to solution
26,475 Views
binli
NXP Employee
NXP Employee

Hi:

My license of S32DS for ARM 2018R1 IDE has expired. Could you help check and extend it for me? 

Thanks.

 

binli_0-1654501988529.png

 

0 Kudos
Reply
1 Solution
26,456 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

I've extended your entitlement. Please refresh or re-activate your installation.

Best Regards,

Mike

View solution in original post

81 Replies
7,320 Views
cjgyf
Contributor II

My license has also expired (9DE8-C6AE-8B6B-952B), could you extend it for me? Thank you very much!

0 Kudos
Reply
7,278 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @cjgyf ,

I've extended your entitlement through end of December 2025. Please refresh or re-activate your installation.

Best Regards,

- Mehul Patel

0 Kudos
Reply
9,021 Views
francesco_solit
Contributor I

Good morning.

Our licence for S32DS for ARM 2018R1 is going to expire. Could you please extend it? You can find it in attachment.

Thank you and kind regards,

Francesco Solito

0 Kudos
Reply
8,878 Views
mikedoidge
NXP Employee
NXP Employee

Hello @francesco_solit,

I have extended your entitlement. Please refresh the license so it will receive the new expiration date.

Best Regards,

Mike

0 Kudos
Reply
8,808 Views
francesco_solit
Contributor I

Thnk you very much mike.

Kind regards,

Francesco Solito

0 Kudos
Reply
8,210 Views
francesco_solit
Contributor I

Hello Mike

The re-activation is now working on my PC, but it is no more working on the other PCs of my colleagues, where in the past the same licence was working. Is it possible to extend the license also for my colleagues? Or is it possible to receive new licences for them? Their NXP accounts are:

federico.bocconi@metasystemcorporation.com

matteo.cocconcelli@metasystem.it

Thank you in advance and kind regards,

Francesco Solito

0 Kudos
Reply
7,831 Views
mikedoidge
NXP Employee
NXP Employee

Hello @francesco_solit,

I checked the server logs for this entitlement. It is reporting the maximum number of returned licenses has been reached. I reset the count, so it should work now. Please ask your colleagues to try again.

Please also note, your colleagues could get their own license if they use the following link and login to their NXP.com account:

https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=S32-DS-ARM_v2018

Best Regards,

Mike

0 Kudos
Reply
7,443 Views
francesco_solit
Contributor I

Hello Mike

Sorry for the delay. Thank you very much. Now everything is working correctly.

Kind regards,

Francesco

0 Kudos
Reply
7,817 Views
NiceHyuny
Contributor I

Hi, my licence is expired, can you help me to extend it?

The number is 

4F70-F0A3-101C-3C96

 

Thank u so much.

0 Kudos
Reply
7,684 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

I have extended this entitlement through 2025. Please use the activation code to receive the new license.

Best Regards,

Mike

0 Kudos
Reply
5,417 Views
Jaydenyzhu
Contributor I

Dear,

my license of S32 Design Studio for ARM Version 2018.R1 has expired. Could you please extend it for me? 

Activation Code D5D0-D801-AB24-58DF

Thanks a lot.

0 Kudos
Reply
5,332 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hello, @Jaydenyzhu 

I have extended this entitlement through 2026.

Please use the activation code to receive the new license.

Best Regards,

- Mehul Patel

0 Kudos
Reply
5,447 Views
Jaydenyzhu
Contributor I

Thank you very much. Now everything is working correctly. Thank you again.

0 Kudos
Reply
8,224 Views
atranzillo93
Contributor III

Hi, my licence is expired, can you help me to extend it?

The number is 

B361-6887-8BBF-ED12

 

Moreover, also for my collegue Anna D'Alessio: 

E735-6A42-FED4-6005

 

Thank u so much.

Anita

0 Kudos
Reply
8,413 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

Both entitlements have been extended through 2025. Please use the activation code to re-activate your installations.

Best Regards,

Mike

0 Kudos
Reply
8,880 Views
valeriaalessi
Contributor II

Good morning,

my license of S32DS for ARM 2018R1 IDE has expired. Could you please extend it for me? 

In attachment you can find the current licence expired.

Thanks a lot.

Valeria

0 Kudos
Reply
8,672 Views
mikedoidge
NXP Employee
NXP Employee

Hello @valeriaalessi,

I checked the license server. It reported that you had exceeded the maximum number of returns. I have reset the return count. The issue should now be resolved. Please try once more.

Mike

0 Kudos
Reply
8,637 Views
valeriaalessi
Contributor II

Good morning,

I tried to re-activate with the same license number but it continues to tell me that the license is for another feature. However, the second error about exceeded number of returns does not come out again, after the first one.

Could you help me?

Thanks a lot.

Valeria

0 Kudos
Reply
8,609 Views
mikedoidge
NXP Employee
NXP Employee

Hello @valeriaalessi,

I have manually returned the license from the server side. When you receive the offer to return the license, please choose 'Yes'. Sometimes there is some setting which does not get reset properly and this will force it to be reset. After this, and with my action to return the license, you should be able to activate without issue.

Best Regards,

Mike

0 Kudos
Reply
8,590 Views
valeriaalessi
Contributor II

Good morning!

The issue is solved!

Thanks a lot.

Valeria

8,660 Views
mikedoidge
NXP Employee
NXP Employee

Hello,

I have extended your license through 2025. Please refresh from the Help->NXP Licenses menu or reactivate using the same activation code as before.

Best Regards,

Mike

0 Kudos
Reply