S32DS download code fail with MPC574XP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS download code fail with MPC574XP

Jump to solution
3,635 Views
jefferson_ll
Contributor III

Hi NXP,

 

I have a problem with S32DS.

 

The following steps could let me enter debug mode and using single step to trace my code well.
Run -> Debug config -> Debug


When I use "Run -> Run as" there are two options Local c/c++ application and S32DS c/c++ pplication.
I select one of them the another window shows C local application and then I select OK.

As show following figure:

169414_169414.jpg20161114_1.jpg

 

The new window shows "Launch MPC5744-Uart_with_DMA-S32DS.elf" has encountered a problem.

As show following figure:

169433_169433.jpg20161114_2.jpg

 

 

I don't know how to solve this problem. Does somebody give me a help?

 

Thank you very much.

Labels (1)
1 Solution
3,361 Views
martin_kovar
NXP Employee
NXP Employee

Hi Jeff,

functionality of this button is not implemented correct. Please use only Debug button to run your application.

Regards,

Martin

View solution in original post

3 Replies
3,362 Views
martin_kovar
NXP Employee
NXP Employee

Hi Jeff,

functionality of this button is not implemented correct. Please use only Debug button to run your application.

Regards,

Martin

3,361 Views
jefferson_ll
Contributor III

Hi Martin Kovar,

According your instruction uses Debug button, I can run code in debug mode and Free run mode.

Thanks for your help.

Best regards,

Jeff

3,361 Views
jefferson_ll
Contributor III

Hi Martin Kovar,

Thanks for your reply.

Could you give me some steps about "Debug button" ?

Are there any other settings missing?

Best regards,

Jeff

0 Kudos
Reply