S32DS download code fail with MPC574XP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS download code fail with MPC574XP

ソリューションへジャンプ
3,689件の閲覧回数
jefferson_ll
Contributor III

Hi NXP,

 

I have a problem with S32DS.

 

The following steps could let me enter debug mode and using single step to trace my code well.
Run -> Debug config -> Debug


When I use "Run -> Run as" there are two options Local c/c++ application and S32DS c/c++ pplication.
I select one of them the another window shows C local application and then I select OK.

As show following figure:

169414_169414.jpg20161114_1.jpg

 

The new window shows "Launch MPC5744-Uart_with_DMA-S32DS.elf" has encountered a problem.

As show following figure:

169433_169433.jpg20161114_2.jpg

 

 

I don't know how to solve this problem. Does somebody give me a help?

 

Thank you very much.

ラベル(1)
1 解決策
3,415件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi Jeff,

functionality of this button is not implemented correct. Please use only Debug button to run your application.

Regards,

Martin

元の投稿で解決策を見る

3 返答(返信)
3,416件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi Jeff,

functionality of this button is not implemented correct. Please use only Debug button to run your application.

Regards,

Martin

3,415件の閲覧回数
jefferson_ll
Contributor III

Hi Martin Kovar,

According your instruction uses Debug button, I can run code in debug mode and Free run mode.

Thanks for your help.

Best regards,

Jeff

3,415件の閲覧回数
jefferson_ll
Contributor III

Hi Martin Kovar,

Thanks for your reply.

Could you give me some steps about "Debug button" ?

Are there any other settings missing?

Best regards,

Jeff

0 件の賞賛
返信