S32DS connect PE Multilink

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS connect PE Multilink

4,541 Views
ronliu
Contributor IV

Hi all,

I have a problem when I'm using S32DS to debug a MPC5x project.

141856_141856.png1.png

141869_141869.png2.png

 

As the pictures show, I don't know why the S32DS aren't able to connect the PE multilink. But it worked well before. This strange problem comes to me only the week. Could you please give me some introduction?

Thanks all.m

Best regards,

Ron

Labels (2)
2 Replies

3,732 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

try to download the newest drivers and update you debugger. Here is the URL:

http://www.pemicro.com/support/download_processor.cfm

Download and install this file:

  P&E Hardware Interface Drivers, Version 12 (Win XP/Vista/7/8/10)

Also look at this thread and try to use the procedure which advises Stanislav.

Eternal "configuring GDB" if P&E Multilink not connected or target OFF

Regards,

Martin

0 Kudos
Reply

3,731 Views
ronliu
Contributor IV

Martin,

Thanks. I create a new project and copy all my code into it. And then the problem is solved.

It seems very strange. But It really works.

Regards,

Ron