S32DS connect PE Multilink

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS connect PE Multilink

4,536件の閲覧回数
ronliu
Contributor IV

Hi all,

I have a problem when I'm using S32DS to debug a MPC5x project.

141856_141856.png1.png

141869_141869.png2.png

 

As the pictures show, I don't know why the S32DS aren't able to connect the PE multilink. But it worked well before. This strange problem comes to me only the week. Could you please give me some introduction?

Thanks all.m

Best regards,

Ron

ラベル(2)
タグ(3)
2 返答(返信)

3,727件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hi,

try to download the newest drivers and update you debugger. Here is the URL:

http://www.pemicro.com/support/download_processor.cfm

Download and install this file:

  P&E Hardware Interface Drivers, Version 12 (Win XP/Vista/7/8/10)

Also look at this thread and try to use the procedure which advises Stanislav.

Eternal "configuring GDB" if P&E Multilink not connected or target OFF

Regards,

Martin

0 件の賞賛
返信

3,726件の閲覧回数
ronliu
Contributor IV

Martin,

Thanks. I create a new project and copy all my code into it. And then the problem is solved.

It seems very strange. But It really works.

Regards,

Ron