S32DS Install Fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS Install Fail

28,393件の閲覧回数
james4
Contributor I

S32DS_ARM_Win32_v2.2 Install Anywhere error

Hi,

 

I failed installs of the S32DS_ARM_Win32_v2.2, on  my PC.

The window asking for activation code is not opening in his case, the installation is just falling back and uninstalling itself.

 

I run the installer using admin rights.

 

 

Attached is the last installation log failure: - it doesn't say much about the cause:

Install Uninstaller: S32 Design Studio for ARM Version 2.2(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

 

Any ideas of what to try next are welcome!

タグ(1)
0 件の賞賛
返信
14 返答(返信)

25,883件の閲覧回数
lei324
Contributor I

Is this issue solved, I'm having the same issue.

0 件の賞賛
返信

25,869件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @lei324,

I checked your installation log file. The errors reported are identical to the log reported the user in this thread:

S32 DS install fail——rolling back - NXP Community

Perhaps his solution works for you?

Best Regards,

Mike

 

0 件の賞賛
返信

27,947件の閲覧回数
james4
Contributor I

1587811122(1).png

In the process of installing,show in the picture,the popup window of activation code couldn't popup and rolled back.What is the problem?

0 件の賞賛
返信

27,947件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello [email protected]‌,

1) You indicated that you run the installer using admin rights. The installation should be conducted from a user account that is part of the administrative rights group, this does NOT mean to execute the installer using the option 'Run As Administrator'. Please confirm that you are meeting this requirement apropriately.

2) If the above admin rights are confirmed, then please check the document: https://community.nxp.com/docs/DOC-345238 The solution here may work for your issue.

Please reply back with your response on the 2 suggestions above.

Best Regards,

Mike

0 件の賞賛
返信

27,947件の閲覧回数
james4
Contributor I

Hello Mike,

   1. I enable my Administrator accout and signed in this accout ,then reinstall   the error is the same.

  2. 

#

# A fatal error has been detected by the Java Runtime Environment:

#

#  EXCEPTION_ACCESS_VIOLATION (0xc0000005) at pc=0x5afc8c19, pid=10540, tid=0x000031a4

#

# JRE version: Java(TM) SE Runtime Environment (8.0_202-b08) (build 1.8.0_202-b08)

# Java VM: Java HotSpot(TM) Client VM (25.202-b08 mixed mode windows-x86 )

# Problematic frame:

# C  [cll_app.dll+0x18c19]

In my install log,there is not this error, anyway   I   delete 'C:\ProgramData\FLEXNet'  and reinstall.The error is also the same.

Any other solution except reinstalling  WIN10?

Thanks!

0 件の賞賛
返信

27,947件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello [email protected]‌,

After further analysis, your issue is cause by missing Microsoft Visual C++ and 2013 Redistributables from Microsoft website. This is supposed to be installed when S32 Design Studio is installed, but it seems it must be failing for some reason. Perhaps you could try to install directly from Microsoft and see if it installs, or if it fails perhaps you can see the reason.

Please try this and let us know if you are successful in completing the S32 Design Studio installation.

Best Regards,

Mike

0 件の賞賛
返信

27,947件の閲覧回数
james4
Contributor I

1588228599(1).png

1588228634(1).png

I download the Microsoft Visual C++ 2013 Redistributalbe from Microsoft websit. When installing it,it indicated I had installed it.

Then reinstall s32ds,the error is the same.

0 件の賞賛
返信

27,947件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello [email protected]‌,

Please check that both 32- and 64-bit redistributables packages are installed. When you get the prompt, please use the 'Repair' button to reinstall.

Best Regards,

Mike

0 件の賞賛
返信

27,947件の閲覧回数
james4
Contributor I

The two vision packages are installed. The error is the same.  I decided use  IAR as  my ide.

0 件の賞賛
返信

27,947件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello [email protected]

Our apologies for the delay in reply. Our experts with the InstallAnywhere tool were on national holidays. They have investigated further and believe this may be similar to another issue which was recently reported and solved. The solution was to start the server service shown below. Could you please check it and see if this resolves the issue?

pastedImage_1.png

Best Regards,

Mike

0 件の賞賛
返信

27,947件の閲覧回数
james4
Contributor I

(マイビデオを表示)

0 件の賞賛
返信

27,947件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello [email protected]‌,

Thank you for posting the video, this is very helpful. I see that the prompt to install MS Visual C is no longer appearing. Could you please send an updated installation log file? It could provide a new clue regarding the issue, if the contents are different than previous.

Thanks,

Mike

0 件の賞賛
返信

27,947件の閲覧回数
james4
Contributor I

Hi Mike,

     The log is blow. Thanks!

______________________________________________________________________

Thu May 07 11:43:02 CST 2020

Free Memory: 23558 kB
Total Memory: 36896 kB

java.class.path:
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData\IAClasses.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData\Execute.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\InstallerData\Execute.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData\Resource1.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\InstallerData\Resource1.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\InstallerData

ZGUtil.CLASS_PATH:
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData\IAClasses.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData\Execute.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData

sun.boot.class.path:
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\resources.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\rt.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\sunrsasign.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\jsse.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\jce.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\charsets.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\jfr.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\classes

java.ext.dirs:
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\ext
C:\Windows\Sun\Java\lib\ext

java.version == 1.8.0_202 (Java 1)
java.vm.name == Java HotSpot(TM) Client VM
java.vm.vendor == Oracle Corporation
java.vm.version == 25.202-b08
java.vm.specification.name == Java Virtual Machine Specification
java.vm.specification.vendor == Oracle Corporation
java.vm.specification.version == 1.8
java.specification.name == Java Platform API Specification
java.specification.vendor == Oracle Corporation
java.specification.version == 1.8
java.vendor == Oracle Corporation
java.vendor.url == http://java.oracle.com/
java.class.version == 52.0
java.library.path == C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\bin;C:\Windows\Sun\Java\bin;C:\Windows\system32;C:\Windows;C:\Program Files (x86)\Common Files\Oracle\Java\javapath;D:\Program Files\VanDyke Software\Clients\;d:\MentorGraphics\9.5PADS\SDD_HOME\common\win32\bin;d:\MentorGraphics\9.5PADS\SDD_HOME\common\win32\lib;d:\MentorGraphics\9.5PADS\MGC_HOME.ixn\bin;d:\MentorGraphics\9.5PADS\MGC_HOME.ixn\lib;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Windows\System32\OpenSSH\;C:\QuickStart;C:\Program Files\Intel\WiFi\bin\;C:\Program Files\Common Files\Intel\WirelessCommon\;D:\Program Files (x86)\Microchip\xc8\v2.10\bin;D:\Program Files (x86)\Microchip\xc32\v2.30\bin;;D:\Program Files\Microchip\xc16\v1.50\bin;C:\Users\thornphoenix\AppData\Local\Microsoft\WindowsApps;d:\MentorGraphics\9.5PADS\SDD_HOME\CAMCAD;d:\Users\thornphoenix\AppData\Local\Programs\Microsoft VS Code\bin;.
java.compiler == null
java.home == C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre
java.io.tmpdir == C:\Users\THORNP~1\AppData\Local\Temp\
os.name == Microsoft Windows 10 Enterprise LTSC
os.arch == x86
os.version == 10.0.17763
path.separator == ;
file.separator == \
file.encoding == GBK
user.name == thornphoenix
user.home == C:\Users\thornphoenix
user.dir == C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows
user.language == en
user.region == null
__________________________________________________________________________

Installed Feature(s) S32DSF of S32 Design Studio for ARM Version 2.2

Install Begin: MAY 7, 2020 11:40:50 AM CST
Install End: MAY 7, 2020 11:42:58 AM CST

Installed by InstallAnywhere 18.0 Professional Build 5608


User Interactions
-----------------


#Choose additional feature(s)
#----------------------------
CHOSEN_FEATURE_LIST=S32DSF
CHOSEN_INSTALL_FEATURE_LIST=S32DSF
CHOSEN_INSTALL_SET=S32 Des

#Choose Install Location
#-----------------------
USER_INSTALL_DIR=C:\\NXP\\S32DS_ARM_v2.2

#Choose Shortcut Folder
#----------------------
USER_SHORTCUTS=C:\\Users\\thornphoenix\\AppData\\Roaming\\Microsoft\\Windows\\Start Menu\\Programs\\NXP S32 Design Studio\\S32 Design Studio for ARM Version 2.2

#Install
#-------
-fileOverwrite_C\:\\NXP\\S32DS_ARM_v2.2\\_S32\ Design\ Studio\ for\ ARM\ Version\ 2.2_installation\\resource\\iawin32.dll=Yes
-fileOverwrite_C\:\\NXP\\S32DS_ARM_v2.2\\_S32\ Design\ Studio\ for\ ARM\ Version\ 2.2_installation\\resource\\win64_32_x64.exe=Yes
-fileOverwrite_C\:\\NXP\\S32DS_ARM_v2.2\\_S32\ Design\ Studio\ for\ ARM\ Version\ 2.2_installation\\resource\\remove.exe=Yes
-fileOverwrite_C\:\\NXP\\S32DS_ARM_v2.2\\_S32\ Design\ Studio\ for\ ARM\ Version\ 2.2_installation\\resource\\invoker.exe=Yes

Summary
-------

Installation: Unsuccessful.

56 Successes
31 Warnings
1 NonFatalErrors
1 FatalErrors

Action Notes:

None

Install Log Detail:

Check Disk Space: C:\NXP\S32DS__v2.2
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space:5,556,923,689 Bytes Free Disk Space:101,440,598,016 Bytes

Check Disk Space: C:\NXP\S32DS_ARM_v2.2
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space:5,556,923,689 Bytes Free Disk Space:101,440,598,016 Bytes

Install Directory: C:\NXP\S32DS_ARM_v2.2\jre
Status: SUCCESSFUL

Install JRE: C:\NXP\S32DS_ARM_v2.2\jre
Status: SUCCESSFUL

Install Directory: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\
Status: SUCCESSFUL
Additional Notes: NOTE - Directory already existed

Execute Command: NET SESSION
Status: SUCCESSFUL


Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\vcredist_2013_x86.exe
Status: SUCCESSFUL

Expand Archive: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\vcredist32.zip
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\vcredist_2010SP1_x86.exe
Status: SUCCESSFUL

Expand Archive: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\vcredist2010.zip
Status: SUCCESSFUL

Execute Command: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\vcredist_2013_x86.exe /quiet
Status: SUCCESSFUL

Execute Command: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\vcredist_2010SP1_x86.exe /quiet
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\clljni.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cllSvrUtility.exe
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cllSvrUtility.exe.manifest
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_app.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_app_libFNP.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_svr.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_svr_libFNP.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\FnpCommsSoap.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\FNP_Act_Installer.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\clljni.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\cll_app.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\cll_app_libFNP.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\cll_svr.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\cll_svr_libFNP.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\FnpCommsSoap.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\FnpCommsSoap.so
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\FNP_Act_Installer.dll
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\libclljni.so
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\libcll_app.so
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\libcll_app_libFNP.so
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\libcll_svr.so
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\libcll_svr_libFNP.so
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\FNPLicensingService\FNPLicensingService
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\install_fnp.sh
Status: SUCCESSFUL

Install File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\license.jar
Status: SUCCESSFUL

Expand Archive: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\Activation.zip
Status: SUCCESSFUL

Execute Command: java "-Djava.library.path=C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86" -jar "C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\license.jar" install -prod S32DS-IDE-ARM_2.2
Status: SUCCESSFUL


Execute Command: java "-Djava.library.path=C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86" -jar "C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\license.jar" verify -feature Activated -version 2.2 -prod S32DS-IDE-ARM_2.2
Status: SUCCESSFUL

Execute Command: java "-Djava.library.path=C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86" -jar "C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\license.jar" run -feature Activated -version 2.2 -prod S32DS-IDE-ARM_2.2
Status: SUCCESSFUL


Execute Command: java "-Djava.library.path=C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86" -jar "C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\license.jar" list
Status: SUCCESSFUL


Install Uninstaller: S32 Design Studio for ARM Version 2.2(Install All Uninstaller Components)
Status: SUCCESSFUL

Install Directory: C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\resource\
Status: SUCCESSFUL

Install File: C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\resource\iawin32.dll
Status: SUCCESSFUL

Install File: C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\resource\win64_32_x64.exe
Status: SUCCESSFUL

Install File: C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\resource\remove.exe
Status: SUCCESSFUL

Install File: C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\resource\invoker.exe
Status: SUCCESSFUL

Install Uninstaller: S32 Design Studio for ARM Version 2.2(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\vcredist_2013_x86.exe
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\vcredist_2010SP1_x86.exe
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\clljni.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cllSvrUtility.exe
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cllSvrUtility.exe.manifest
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_app.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_app_libFNP.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_svr.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_svr_libFNP.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\FnpCommsSoap.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\FNP_Act_Installer.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\clljni.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\cll_app.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\cll_app_libFNP.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\cll_svr.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\cll_svr_libFNP.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\FnpCommsSoap.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\FnpCommsSoap.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\FNP_Act_Installer.dll
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\libclljni.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\libcll_app.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\libcll_app_libFNP.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\libcll_svr.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64\libcll_svr_libFNP.so
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\FNPLicensingService\FNPLicensingService
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\install_fnp.sh
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall File: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\license.jar
Status: WARNING
Additional Notes: WARNING - The file does not exist

Uninstall Folder: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\FNPLicensingService
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\x64
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll
Status: WARNING
Additional Notes: WARNING - The path does not exist

Uninstall Folder: C:\NXP\S32DS_ARM_v2.2\jre
Status: SUCCESSFUL

Remove Registry Entry: 5 HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\null
Status: SUCCESSFUL

Error occurred while installing the following Action, hence rolling back the installation....!


Action Name: Trigger Rollback Action
Action Description: Trigger Rollback Action


Error Details as below:


This action rolls back the Installation.
====================STDERR ENTRIES==================

__________________________________________________________________________

InstallAnywhere 2017
Version: 18.0
__________________________________________________________________________

Thu May 07 11:40:46 CST 2020

Free Memory: 12692 kB
Total Memory: 15872 kB

No Arguments

java.class.path:
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData\IAClasses.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData\Execute.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\InstallerData\Execute.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData\Resource1.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\InstallerData\Resource1.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\InstallerData

ZGUtil.CLASS_PATH:
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData\IAClasses.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData\Execute.zip
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\InstallerData

sun.boot.class.path:
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\resources.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\rt.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\sunrsasign.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\jsse.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\jce.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\charsets.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\jfr.jar
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\classes

java.ext.dirs:
C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\lib\ext
C:\Windows\Sun\Java\lib\ext

java.version == 1.8.0_202 (Java 1)
java.vm.name == Java HotSpot(TM) Client VM
java.vm.vendor == Oracle Corporation
java.vm.version == 25.202-b08
java.vm.specification.name == Java Virtual Machine Specification
java.vm.specification.vendor == Oracle Corporation
java.vm.specification.version == 1.8
java.specification.name == Java Platform API Specification
java.specification.vendor == Oracle Corporation
java.specification.version == 1.8
java.vendor == Oracle Corporation
java.vendor.url == http://java.oracle.com/
java.class.version == 52.0
java.library.path == C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre\bin;C:\Windows\Sun\Java\bin;C:\Windows\system32;C:\Windows;C:\Program Files (x86)\Common Files\Oracle\Java\javapath;D:\Program Files\VanDyke Software\Clients\;d:\MentorGraphics\9.5PADS\SDD_HOME\common\win32\bin;d:\MentorGraphics\9.5PADS\SDD_HOME\common\win32\lib;d:\MentorGraphics\9.5PADS\MGC_HOME.ixn\bin;d:\MentorGraphics\9.5PADS\MGC_HOME.ixn\lib;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Windows\System32\OpenSSH\;C:\QuickStart;C:\Program Files\Intel\WiFi\bin\;C:\Program Files\Common Files\Intel\WirelessCommon\;D:\Program Files (x86)\Microchip\xc8\v2.10\bin;D:\Program Files (x86)\Microchip\xc32\v2.30\bin;;D:\Program Files\Microchip\xc16\v1.50\bin;C:\Users\thornphoenix\AppData\Local\Microsoft\WindowsApps;d:\MentorGraphics\9.5PADS\SDD_HOME\CAMCAD;d:\Users\thornphoenix\AppData\Local\Programs\Microsoft VS Code\bin;.
java.compiler == null
java.home == C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows\resource\jre
java.io.tmpdir == C:\Users\THORNP~1\AppData\Local\Temp\
os.name == Microsoft Windows 10 Enterprise LTSC
os.arch == x86
os.version == 10.0.17763
path.separator == ;
file.separator == \
file.encoding == GBK
user.name == thornphoenix
user.home == C:\Users\thornphoenix
user.dir == C:\Users\thornphoenix\AppData\Local\Temp\I1588822722\Windows
user.language == en
user.region == null
__________________________________________________________________________


Loading externalized properties

ZGGfxUtil.loadImage: loading failed for:
com/zerog/ia/installer/images/billboard_defaultNew.png
RepositoryManager: Trying fallback repository location...
#
# INSTALLING VM: C:\NXP\S32DS_ARM_v2.2\jre
#
System's temporary directory = C:\Users\thornphoenix\AppData\Local\Temp
==== NET SESSION command log start: ====
Returned: 0
Console: There are no entries in the list.


Errors:
==== NET SESSION command log end. ====
==== License service installation log start: ====
Console:
Errors: Exception in thread "main" java.lang.UnsatisfiedLinkError: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_app.dll: Can't find dependent libraries
at java.lang.ClassLoader$NativeLibrary.load(Native Method)
at java.lang.ClassLoader.loadLibrary0(ClassLoader.java:1941)
at java.lang.ClassLoader.loadLibrary(ClassLoader.java:1857)
at java.lang.Runtime.loadLibrary0(Runtime.java:870)
at java.lang.System.loadLibrary(System.java:1122)
at com.nxp.s32ds.ext.rcp.license.cll.CLL.<init>(CLL.java:18)
at com.nxp.s32ds.ext.rcp.license.cll.CLL.loadCLL(CLL.java:8)
at com.nxp.s32ds.rcp.license.core.cli.CLI.execute(CLI.java:39)
at com.nxp.s32ds.rcp.license.core.cli.CLI.main(CLI.java:33)

==== License service installation log end. ====
==== License activation log start: ====
Console:
Errors: Exception in thread "main" java.lang.UnsatisfiedLinkError: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_app.dll: Can't find dependent libraries
at java.lang.ClassLoader$NativeLibrary.load(Native Method)
at java.lang.ClassLoader.loadLibrary0(ClassLoader.java:1941)
at java.lang.ClassLoader.loadLibrary(ClassLoader.java:1857)
at java.lang.Runtime.loadLibrary0(Runtime.java:870)
at java.lang.System.loadLibrary(System.java:1122)
at com.nxp.s32ds.ext.rcp.license.cll.CLL.<init>(CLL.java:18)
at com.nxp.s32ds.ext.rcp.license.cll.CLL.loadCLL(CLL.java:8)
at com.nxp.s32ds.rcp.license.core.cli.CLI.execute(CLI.java:39)
at com.nxp.s32ds.rcp.license.core.cli.CLI.main(CLI.java:33)

==== License activation log end. ====
==== License list start: ====
Console:
Errors: Exception in thread "main" java.lang.UnsatisfiedLinkError: C:\Users\thornphoenix\AppData\Local\Temp\848891.tmp\cll\i86\cll_app.dll: Can't find dependent libraries
at java.lang.ClassLoader$NativeLibrary.load(Native Method)
at java.lang.ClassLoader.loadLibrary0(ClassLoader.java:1941)
at java.lang.ClassLoader.loadLibrary(ClassLoader.java:1857)
at java.lang.Runtime.loadLibrary0(Runtime.java:870)
at java.lang.System.loadLibrary(System.java:1122)
at com.nxp.s32ds.ext.rcp.license.cll.CLL.<init>(CLL.java:18)
at com.nxp.s32ds.ext.rcp.license.cll.CLL.loadCLL(CLL.java:8)
at com.nxp.s32ds.rcp.license.core.cli.CLI.execute(CLI.java:39)
at com.nxp.s32ds.rcp.license.core.cli.CLI.main(CLI.java:33)

==== License list end. ====
XMLScriptWriter: No Installation Objects were skipped
8. final log file name=C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_05_07_2020_11_43_02.log

====================STDOUT ENTRIES==================

C:\NXP\S32DS_ARM_v2.2\jre
C:\NXP\S32DS_ARM_v2.2\jre\bin
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-console-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-datetime-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-debug-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-errorhandling-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-file-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-file-l1-2-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-file-l2-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-handle-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-heap-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-interlocked-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-libraryloader-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-localization-l1-2-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-memory-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-namedpipe-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-processenvironment-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-processthreads-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-processthreads-l1-1-1.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-profile-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-rtlsupport-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-string-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-synch-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-synch-l1-2-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-sysinfo-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-timezone-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-core-util-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-conio-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-convert-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-environment-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-filesystem-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-heap-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-locale-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-math-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-multibyte-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-private-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-process-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-runtime-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-stdio-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-string-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-time-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\api-ms-win-crt-utility-l1-1-0.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\awt.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\bci.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\client
C:\NXP\S32DS_ARM_v2.2\jre\bin\client\jvm.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\client\Xusage.txt
C:\NXP\S32DS_ARM_v2.2\jre\bin\concrt140.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\dcpr.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\decora_sse.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\deploy.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\dtplugin
C:\NXP\S32DS_ARM_v2.2\jre\bin\dtplugin\deployJava1.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\dtplugin\npdeployJava1.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\dt_shmem.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\dt_socket.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\eula.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\fontmanager.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\fxplugins.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\glass.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\glib-lite.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\gstreamer-lite.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\hprof.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\instrument.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\j2pcsc.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\j2pkcs11.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jaas_nt.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jabswitch.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\java-rmi.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\java.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\java.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\JavaAccessBridge-32.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\JavaAccessBridge.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\javacpl.cpl
C:\NXP\S32DS_ARM_v2.2\jre\bin\javacpl.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\javafx_font.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\javafx_font_t2k.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\javafx_iio.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\javaw.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\javaws.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\java_crw_demo.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jawt.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\JAWTAccessBridge-32.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\JAWTAccessBridge.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jdwp.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jfr.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jfxmedia.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jfxwebkit.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jjs.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\jli.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jp2iexp.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jp2launcher.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\jp2native.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jp2ssv.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jpeg.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jsdt.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jsound.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\jsoundds.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\keytool.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\kinit.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\klist.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\ktab.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\lcms.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\management.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\mlib_image.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\msvcp140.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\msvcr100.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\net.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\nio.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\npt.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\orbd.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\pack200.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\plugin2
C:\NXP\S32DS_ARM_v2.2\jre\bin\plugin2\msvcr100.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\plugin2\npjp2.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\policytool.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\prism_common.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\prism_d3d.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\prism_sw.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\resource.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\rmid.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\rmiregistry.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\servertool.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\splashscreen.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\ssv.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\ssvagent.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\sunec.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\sunmscapi.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\t2k.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\tnameserv.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\ucrtbase.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\unpack.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\unpack200.exe
C:\NXP\S32DS_ARM_v2.2\jre\bin\vcruntime140.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\verify.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\w2k_lsa_auth.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\WindowsAccessBridge-32.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\WindowsAccessBridge.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\wsdetect.dll
C:\NXP\S32DS_ARM_v2.2\jre\bin\zip.dll
C:\NXP\S32DS_ARM_v2.2\jre\COPYRIGHT
C:\NXP\S32DS_ARM_v2.2\jre\lib
C:\NXP\S32DS_ARM_v2.2\jre\lib\accessibility.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\calendars.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\charsets.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\classlist
C:\NXP\S32DS_ARM_v2.2\jre\lib\cmm
C:\NXP\S32DS_ARM_v2.2\jre\lib\cmm\CIEXYZ.pf
C:\NXP\S32DS_ARM_v2.2\jre\lib\cmm\GRAY.pf
C:\NXP\S32DS_ARM_v2.2\jre\lib\cmm\LINEAR_RGB.pf
C:\NXP\S32DS_ARM_v2.2\jre\lib\cmm\PYCC.pf
C:\NXP\S32DS_ARM_v2.2\jre\lib\cmm\sRGB.pf
C:\NXP\S32DS_ARM_v2.2\jre\lib\content-types.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\currency.data
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\ffjcext.zip
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_de.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_es.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_fr.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_it.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_ja.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_ko.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_pt_BR.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_sv.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_zh_CN.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_zh_HK.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\messages_zh_TW.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\splash.gif
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\[email protected]
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\splash_11-lic.gif
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy\[email protected]
C:\NXP\S32DS_ARM_v2.2\jre\lib\deploy.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\access-bridge-32.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\access-bridge.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\cldrdata.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\dnsns.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\jaccess.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\jfxrt.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\localedata.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\meta-index
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\nashorn.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\sunec.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\sunjce_provider.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\sunmscapi.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\sunpkcs11.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\ext\zipfs.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\flavormap.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\fontconfig.bfc
C:\NXP\S32DS_ARM_v2.2\jre\lib\fontconfig.properties.src
C:\NXP\S32DS_ARM_v2.2\jre\lib\fonts
C:\NXP\S32DS_ARM_v2.2\jre\lib\fonts\LucidaBrightDemiBold.ttf
C:\NXP\S32DS_ARM_v2.2\jre\lib\fonts\LucidaBrightDemiItalic.ttf
C:\NXP\S32DS_ARM_v2.2\jre\lib\fonts\LucidaBrightItalic.ttf
C:\NXP\S32DS_ARM_v2.2\jre\lib\fonts\LucidaBrightRegular.ttf
C:\NXP\S32DS_ARM_v2.2\jre\lib\fonts\LucidaSansDemiBold.ttf
C:\NXP\S32DS_ARM_v2.2\jre\lib\fonts\LucidaSansRegular.ttf
C:\NXP\S32DS_ARM_v2.2\jre\lib\fonts\LucidaTypewriterBold.ttf
C:\NXP\S32DS_ARM_v2.2\jre\lib\fonts\LucidaTypewriterRegular.ttf
C:\NXP\S32DS_ARM_v2.2\jre\lib\hijrah-config-umalqura.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\i386
C:\NXP\S32DS_ARM_v2.2\jre\lib\i386\jvm.cfg
C:\NXP\S32DS_ARM_v2.2\jre\lib\images
C:\NXP\S32DS_ARM_v2.2\jre\lib\images\cursors
C:\NXP\S32DS_ARM_v2.2\jre\lib\images\cursors\cursors.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\images\cursors\invalid32x32.gif
C:\NXP\S32DS_ARM_v2.2\jre\lib\images\cursors\win32_CopyDrop32x32.gif
C:\NXP\S32DS_ARM_v2.2\jre\lib\images\cursors\win32_CopyNoDrop32x32.gif
C:\NXP\S32DS_ARM_v2.2\jre\lib\images\cursors\win32_LinkDrop32x32.gif
C:\NXP\S32DS_ARM_v2.2\jre\lib\images\cursors\win32_LinkNoDrop32x32.gif
C:\NXP\S32DS_ARM_v2.2\jre\lib\images\cursors\win32_MoveDrop32x32.gif
C:\NXP\S32DS_ARM_v2.2\jre\lib\images\cursors\win32_MoveNoDrop32x32.gif
C:\NXP\S32DS_ARM_v2.2\jre\lib\javafx.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\javaws.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\jce.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\jfr
C:\NXP\S32DS_ARM_v2.2\jre\lib\jfr\default.jfc
C:\NXP\S32DS_ARM_v2.2\jre\lib\jfr\profile.jfc
C:\NXP\S32DS_ARM_v2.2\jre\lib\jfr.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\jfxswt.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\jsse.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\jvm.hprof.txt
C:\NXP\S32DS_ARM_v2.2\jre\lib\logging.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\management
C:\NXP\S32DS_ARM_v2.2\jre\lib\management\jmxremote.access
C:\NXP\S32DS_ARM_v2.2\jre\lib\management\jmxremote.password.template
C:\NXP\S32DS_ARM_v2.2\jre\lib\management\management.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\management\snmp.acl.template
C:\NXP\S32DS_ARM_v2.2\jre\lib\management-agent.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\meta-index
C:\NXP\S32DS_ARM_v2.2\jre\lib\net.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\plugin.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\psfont.properties.ja
C:\NXP\S32DS_ARM_v2.2\jre\lib\psfontj2d.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\resources.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\rt.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\security
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\blacklist
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\blacklisted.certs
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\cacerts
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\java.policy
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\java.security
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\javaws.policy
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\policy
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\policy\limited
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\policy\limited\local_policy.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\policy\limited\US_export_policy.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\policy\unlimited
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\policy\unlimited\local_policy.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\policy\unlimited\US_export_policy.jar
C:\NXP\S32DS_ARM_v2.2\jre\lib\security\trusted.libraries
C:\NXP\S32DS_ARM_v2.2\jre\lib\sound.properties
C:\NXP\S32DS_ARM_v2.2\jre\lib\tzdb.dat
C:\NXP\S32DS_ARM_v2.2\jre\lib\tzmappings
C:\NXP\S32DS_ARM_v2.2\jre\LICENSE
C:\NXP\S32DS_ARM_v2.2\jre\README.txt
C:\NXP\S32DS_ARM_v2.2\jre\release
C:\NXP\S32DS_ARM_v2.2\jre\THIRDPARTYLICENSEREADME-JAVAFX.txt
C:\NXP\S32DS_ARM_v2.2\jre\THIRDPARTYLICENSEREADME.txt
C:\NXP\S32DS_ARM_v2.2\jre\Welcome.html
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\.com.zerog.registry.xml
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\InstallScript.iap_xml
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_24_2020_23_57_01.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_25_2020_00_12_27.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_25_2020_00_41_02.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_25_2020_00_45_59.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_25_2020_17_20_36.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_25_2020_17_43_29.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_25_2020_18_06_06.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_26_2020_19_21_51.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_28_2020_10_30_15.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_28_2020_10_53_56.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_04_30_2020_14_45_09.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\Logs\S32_Design_Studio_for_ARM_Version_2.2_Install_05_07_2020_11_36_46.log
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\resource
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\resource\iawin32.dll
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\resource\invoker.exe
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\resource\remove.exe
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\resource\win64_32_x64.exe
C:\NXP\S32DS_ARM_v2.2\_S32 Design Studio for ARM Version 2.2_installation\uninstaller.jar

0 件の賞賛
返信

27,947件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello [email protected]‌,

The new log appears to be same as previous, so no new details are to be learned from it.

I can assure you that this is not a usual type of problem. Most of the few problems encountered by our users are solved by the steps I shared with you earlier.

Before installing S32 Design Studio, was your PC a fresh installation of the Windows OS? It is possible that some services are missing which we would normally expect to already be installed.

Our experts have suggested that it might be necessary to perform an investigation using the tool 'dependency walker'. Please see the following steps:

Deeper steps could require Dependency Walker https://en.wikipedia.org/wiki/Dependency_Walker

 

You can suggest to investigate the problematic DLL with 32-bit DW:
pastedImage_1.png
pastedImage_2.png

Although, obtaining that DLL could be tricky, e.g.:

pastedImage_3.png

pastedImage_4.png

pastedImage_5.png

pastedImage_6.png

Best Regards and Stay Safe,

Mike

0 件の賞賛
返信