S32DS - ISELED example load error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS - ISELED example load error

ソリューションへジャンプ
2,447件の閲覧回数
ssean
Contributor IV

Hello.

I created ISELED example.

ssean_0-1746161691326.pngssean_0-1746161691326.png

 

When I load this project, S32DS popup error message.

ssean_1-1746161763029.pngssean_1-1746161763029.png

 

How can I load this project ?

 

S32DS v3.5

 

 

タグ(1)
0 件の賞賛
返信
1 解決策
2,322件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ssean 

The example you shared is the most recent one, so the best option is to create a new project with the right RTD version. Then, just copy the application source files from the pre-existing project, along with any customizations of the project properties.

Sorry for the inconvenience.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
2,417件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ssean 

Could you please verify that you have correctly installed S32K3 RTD 4.0.0? This version is required for S32K3 ISELED R21-11 2.0.0.

 

BR, VaneB

0 件の賞賛
返信
2,363件の閲覧回数
ssean
Contributor IV

Hello @VaneB 

Here is my installed RTD list.

I have RTD 3.0 and 4.0.

ssean_0-1746572976295.pngssean_0-1746572976295.png

 

BRs,

Sean Sung

タグ(1)
0 件の賞賛
返信
2,345件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ssean 

According to the information provided about the installed packages, it seems that you have several RTD versions installed in your S32DS instance. To rule out a possible cause related to a package conflict, could you please uninstall all the packages and only reinstall the RTD version 4.0.0?

0 件の賞賛
返信
2,339件の閲覧回数
ssean
Contributor IV

Hi @VaneB 

After deleting all RTDs and reinstalling version 4.0, the ISELED project can be loaded.
I also need to load both the ISELED and RTC wakeup examples— is there a way to do this?

Is there an RTC wakeup example available using RTD 4.0 for the S32K312?
Or, is it possible to convert the following project to be compatible with RTD 4.0?

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-STANDBY-wake-up-using-RTC-DS3-5-RTD...

BRs,

Sean Sung

タグ(1)
0 件の賞賛
返信
2,323件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @ssean 

The example you shared is the most recent one, so the best option is to create a new project with the right RTD version. Then, just copy the application source files from the pre-existing project, along with any customizations of the project properties.

Sorry for the inconvenience.

0 件の賞賛
返信
2,307件の閲覧回数
ssean
Contributor IV
Thank you for support.
0 件の賞賛
返信