S32DS - ISELED example load error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS - ISELED example load error

Jump to solution
2,445 Views
ssean
Contributor IV

Hello.

I created ISELED example.

ssean_0-1746161691326.pngssean_0-1746161691326.png

 

When I load this project, S32DS popup error message.

ssean_1-1746161763029.pngssean_1-1746161763029.png

 

How can I load this project ?

 

S32DS v3.5

 

 

Tags (1)
0 Kudos
Reply
1 Solution
2,320 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ssean 

The example you shared is the most recent one, so the best option is to create a new project with the right RTD version. Then, just copy the application source files from the pre-existing project, along with any customizations of the project properties.

Sorry for the inconvenience.

View solution in original post

0 Kudos
Reply
6 Replies
2,415 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ssean 

Could you please verify that you have correctly installed S32K3 RTD 4.0.0? This version is required for S32K3 ISELED R21-11 2.0.0.

 

BR, VaneB

0 Kudos
Reply
2,361 Views
ssean
Contributor IV

Hello @VaneB 

Here is my installed RTD list.

I have RTD 3.0 and 4.0.

ssean_0-1746572976295.pngssean_0-1746572976295.png

 

BRs,

Sean Sung

Tags (1)
0 Kudos
Reply
2,343 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ssean 

According to the information provided about the installed packages, it seems that you have several RTD versions installed in your S32DS instance. To rule out a possible cause related to a package conflict, could you please uninstall all the packages and only reinstall the RTD version 4.0.0?

0 Kudos
Reply
2,337 Views
ssean
Contributor IV

Hi @VaneB 

After deleting all RTDs and reinstalling version 4.0, the ISELED project can be loaded.
I also need to load both the ISELED and RTC wakeup examples— is there a way to do this?

Is there an RTC wakeup example available using RTD 4.0 for the S32K312?
Or, is it possible to convert the following project to be compatible with RTD 4.0?

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-STANDBY-wake-up-using-RTC-DS3-5-RTD...

BRs,

Sean Sung

Tags (1)
0 Kudos
Reply
2,321 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @ssean 

The example you shared is the most recent one, so the best option is to create a new project with the right RTD version. Then, just copy the application source files from the pre-existing project, along with any customizations of the project properties.

Sorry for the inconvenience.

0 Kudos
Reply
2,305 Views
ssean
Contributor IV
Thank you for support.
0 Kudos
Reply