S32DS ARM2.2 and S32K144 Debug configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS ARM2.2 and S32K144 Debug configuration

Jump to solution
2,192 Views
JOE_1209
Contributor III

Hi ,

I created a new project for S32K144, and there are three Target Device for S32K144. The default setting is S32K144F512M15. I am wondering what is different between the three settings. I cannot seem to find any related document. The only one I found is part number on the page 9 of S32K-DS_Data Sheet, but the format is not specified as the name below.

question.PNG

Regards,

Joe

0 Kudos
Reply
1 Solution
2,187 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JOE,

The different between S32K144F512M15 and S32K144F512M150N77P can be found here:https://community.nxp.com/t5/S32K/What-difference-between-S32K-0N47T-and-0N77P/m-p/628450

S32K144WF512M8 should refer to S32K144W AEC-Q100 Grade 0 qualified (-40° C to +150° C Ta)

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
3 Replies
2,165 Views
JOE_1209
Contributor III

Hi Robin,

Thank you for the reply

I see the wording on my chip is FS32K144HFVLH0N57U, is it fine to use Device S32K144F512M15?

The LH should be V, M ,W for temperature rating according to datasheet

 

Regards,

joe

0 Kudos
Reply
2,162 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

You are correct. It's fine to use Device S32K144F512M15 on chip FS32K144HFVLH0N57U.

0 Kudos
Reply
2,188 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JOE,

The different between S32K144F512M15 and S32K144F512M150N77P can be found here:https://community.nxp.com/t5/S32K/What-difference-between-S32K-0N47T-and-0N77P/m-p/628450

S32K144WF512M8 should refer to S32K144W AEC-Q100 Grade 0 qualified (-40° C to +150° C Ta)

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply