S32DS 3.5_RTD3.0.0_S32K344_添加QSPI出错

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS 3.5_RTD3.0.0_S32K344_添加QSPI出错

1,412 Views
harryoceana
Contributor II

S32DS 3.5_RTD3.0.0_S32K344_添加QSPI出错

应该怎样才能正确添加QSPI呢?

harryoceana_0-1719379301791.png

 

0 Kudos
Reply
3 Replies

1,398 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @harryoceana,

This issue is probably caused by a faulty installation. Could you confirm the RTD package is installed correctly? Try importing the Qspi example firstly:

Julin_AragnM_0-1719424599771.png

Julin_AragnM_1-1719424633539.png

Best regards,
Julián

0 Kudos
Reply

1,378 Views
harryoceana
Contributor II

https://community.nxp.com/t5/S32K/S32K344-RMII-QSPI/m-p/1416828

In this post, can't RMII and QSPI be used at the same time, and can't 257BGA package be used at the same time?

Can RMII and QSPI be used at the same time if the chip pin meets the requirement of using RMII and QSPI at the same time?

harryoceana_0-1719552979254.png

harryoceana_1-1719553024367.png

 

 

0 Kudos
Reply

1,336 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @harryoceana,

As you mentioned due to the pad type support RMII + QPSI is not possible for S32K344 devices. It is the same as it is not related to the package. You can look at the tab in the "S32K344_IOMUX.xlsx", where the ethernet use cases are listed:

Julin_AragnM_0-1719950916207.png

Best regards,
Julián

0 Kudos
Reply