S32K344 RMII + QSPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,923件の閲覧回数
marcoelia
Contributor I

Is it really possible to use at the same time both QSPI and RMII interfaces on S32K344 MQFP172?

According to S32K3X4EVB-Q172 schematics/notes the answer seems to be yes.

But, checking the IOMUX spreadsheet, this part seems to lack of medium or fast pads and/or having a bad multiplexing: after selecting the fixed alternatives needed for the 6 QSPI signals, the RMII outputs TXEN, TXD1:0 can be only mapped to 25 MHz max standard-plus pads.

Any suggestion on what is wrong?

0 件の賞賛
返信
1 解決策
3,892件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Marco,

here is the response:

"The S32K344EVB-Q172 was developed to support most of the functionalities of the MCU, on this time the Ethernet has routed the recommendation on the RM to support QSPI + MII. As you mentioned due to the pad type support RMII + QPSI is not possible for S32K344 devices."

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,893件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Marco,

here is the response:

"The S32K344EVB-Q172 was developed to support most of the functionalities of the MCU, on this time the Ethernet has routed the recommendation on the RM to support QSPI + MII. As you mentioned due to the pad type support RMII + QPSI is not possible for S32K344 devices."

Regards,

Lukas

0 件の賞賛
返信
2,817件の閲覧回数
Fast
Contributor IV

Is this still the case, has silicon been improved?

 

0 件の賞賛
返信
3,909件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Marco,

let me check this. I will let you know the result later.

Regards,

Lukas

0 件の賞賛
返信