S32 Design Studio for S32 Platform Error Selecting Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for S32 Platform Error Selecting Project

7,389 Views
andyknitt
Contributor II

I've somehow managed to mess up S32 Design Studio for S32 Platform and am no longer able to select/view my project.  Here's how I got to where I'm at:

  1. Opened/imported the S32K142_CAN_bootloader project from the Unified Bootloader Framework installation package
  2. Made a few minor code edits, have it building successfully
  3. Opened the ConfigTools => Pins menus selection to try to view pin mapping/configuration
  4. Found that there was nothing in this view...apparently this GUI tool hadn't been used to generate the pin configuration code (although the C files for pin configuration were in the "generated code" folder structure - so what was used to generate them?).  When I go to "Config Tools Overview" I get a popup telling me that there is no configuration created yet.  
  5. After opening the Pins view, I get a red error in the toolbar telling me "MCU is not selected"
  6. When I try to open my project using the toolbar I get an error popup that simply says "null" (see below)
  7. The project still appears to build but for the life of me I can't figure out how to get back to the "original" GUI layout with the project structure window, etc.  I appear to be stuck in the ConfigTools screens and can't get out of them.  

I've got to be missing something really simple here but can't figure it out.  Any advice is appreciated.

Thanks,

Andy

andyknitt_0-1626800799425.png

 

0 Kudos
Reply
6 Replies

7,298 Views
mikedoidge
NXP Employee
NXP Employee

Hi Andy,

If your main goal is just to get the screens back the way they were, then use the menu command 'Reset Perspective':

image.png

As for the migration of the project, I'm afraid @jiri_kral is correct. It was created for ProcessorExpert so there may be some work involved to reproduce the same settings within S32 Configuration Tools.

Hope it helps,

Mike

0 Kudos
Reply

7,358 Views
mikedoidge
NXP Employee
NXP Employee

Hi Andy,

You might try converting the project as shown in the video:

Migrating S32K1 projects from S32DS for ARM and SD... - NXP Community

Best Regards,

Mike

0 Kudos
Reply

7,297 Views
andyknitt
Contributor II

Thanks Mike.  I did the migration but am getting build errors.  It seems like some of the files from the original project aren't being found.  Any ideas?

 

17:05:03 **** Incremental Build of configuration Debug for project S32K142_CAN_bootloader ****
make -j12 all
Building file: ../src/driver/flash/src/flash.c
Building file: ../src/driver/flash/src/flash_cfg.c
Building file: ../src/main.c
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@src/driver/flash/src/flash.args" -MMD -MP -MF"src/driver/flash/src/flash.d" -MT"src/driver/flash/src/flash.o" -o "src/driver/flash/src/flash.o" "../src/driver/flash/src/flash.c"
arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"
Invoking: Standard S32DS C Compiler
Building file: ../SDK/rtos/osif/osif_baremetal.c
arm-none-eabi-gcc "@src/driver/flash/src/flash.args" -MMD -MP -MF"src/driver/flash/src/flash_cfg.d" -MT"src/driver/flash/src/flash_cfg.o" -o "src/driver/flash/src/flash_cfg.o" "../src/driver/flash/src/flash_cfg.c"
Building file: ../SDK/platform/pal/src/can/can_pal.c
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/rtos/osif/osif_baremetal.args" -MMD -MP -MF"SDK/rtos/osif/osif_baremetal.d" -MT"SDK/rtos/osif/osif_baremetal.o" -o "SDK/rtos/osif/osif_baremetal.o" "../SDK/rtos/osif/osif_baremetal.c"
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/platform/pal/src/can/can_pal.args" -MMD -MP -MF"SDK/platform/pal/src/can/can_pal.d" -MT"SDK/platform/pal/src/can/can_pal.o" -o "SDK/platform/pal/src/can/can_pal.o" "../SDK/platform/pal/src/can/can_pal.c"
Building file: ../SDK/platform/drivers/src/wdog/wdog_hw_access.c
Building file: ../SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.c
Building file: ../SDK/platform/drivers/src/wdog/wdog_driver.c
Building file: ../SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.c
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.args" -MMD -MP -MF"SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.d" -MT"SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.o" -o "SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.o" "../SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.c"
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/platform/drivers/src/wdog/wdog_driver.args" -MMD -MP -MF"SDK/platform/drivers/src/wdog/wdog_driver.d" -MT"SDK/platform/drivers/src/wdog/wdog_driver.o" -o "SDK/platform/drivers/src/wdog/wdog_driver.o" "../SDK/platform/drivers/src/wdog/wdog_driver.c"
arm-none-eabi-gcc "@SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.args" -MMD -MP -MF"SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.d" -MT"SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.o" -o "SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.o" "../SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.c"
../src/driver/flash/src/flash.c:2:27: fatal error: flash_hal_Cfg.h: No such file or directory
#include "flash_hal_Cfg.h"
^
compilation terminated.
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/platform/drivers/src/wdog/wdog_driver.args" -MMD -MP -MF"SDK/platform/drivers/src/wdog/wdog_hw_access.d" -MT"SDK/platform/drivers/src/wdog/wdog_hw_access.o" -o "SDK/platform/drivers/src/wdog/wdog_hw_access.o" "../SDK/platform/drivers/src/wdog/wdog_hw_access.c"
Building file: ../SDK/platform/drivers/src/power/power_manager.c
make: *** [src/driver/flash/src/subdir.mk:23: src/driver/flash/src/flash.o] Error 1
make: *** Waiting for unfinished jobs....
../src/main.c:28:29: fatal error: bootloader_main.h: No such file or directory
#include "bootloader_main.h"
^
compilation terminated.
Invoking: Standard S32DS C Compiler
Finished building: ../src/driver/flash/src/flash_cfg.c
arm-none-eabi-gcc "@SDK/platform/drivers/src/power/power_manager.args" -MMD -MP -MF"SDK/platform/drivers/src/power/power_manager.d" -MT"SDK/platform/drivers/src/power/power_manager.o" -o "SDK/platform/drivers/src/power/power_manager.o" "../SDK/platform/drivers/src/power/power_manager.c"
make: *** [src/subdir.mk:20: src/main.o] Error 1

Finished building: ../SDK/rtos/osif/osif_baremetal.c

Finished building: ../SDK/platform/pal/src/can/can_pal.c

Finished building: ../SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.c
Finished building: ../SDK/platform/drivers/src/wdog/wdog_driver.c
Finished building: ../SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.c


Finished building: ../SDK/platform/drivers/src/wdog/wdog_hw_access.c


Finished building: ../SDK/platform/drivers/src/power/power_manager.c

"make -j12 all" terminated with exit code 2. Build might be incomplete.

17:05:05 Build Failed. 5 errors, 0 warnings. (took 2s.504ms)

 

0 Kudos
Reply

7,296 Views
andyknitt
Contributor II

Thanks Mike.  I tried this but the build fails after the migration, it seems like it can't find some .h files from the original project.  

17:05:03 **** Incremental Build of configuration Debug for project S32K142_CAN_bootloader ****
make -j12 all
Building file: ../src/driver/flash/src/flash.c
Building file: ../src/driver/flash/src/flash_cfg.c
Building file: ../src/main.c
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@src/driver/flash/src/flash.args" -MMD -MP -MF"src/driver/flash/src/flash.d" -MT"src/driver/flash/src/flash.o" -o "src/driver/flash/src/flash.o" "../src/driver/flash/src/flash.c"
arm-none-eabi-gcc "@src/main.args" -MMD -MP -MF"src/main.d" -MT"src/main.o" -o "src/main.o" "../src/main.c"
Invoking: Standard S32DS C Compiler
Building file: ../SDK/rtos/osif/osif_baremetal.c
arm-none-eabi-gcc "@src/driver/flash/src/flash.args" -MMD -MP -MF"src/driver/flash/src/flash_cfg.d" -MT"src/driver/flash/src/flash_cfg.o" -o "src/driver/flash/src/flash_cfg.o" "../src/driver/flash/src/flash_cfg.c"
Building file: ../SDK/platform/pal/src/can/can_pal.c
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/rtos/osif/osif_baremetal.args" -MMD -MP -MF"SDK/rtos/osif/osif_baremetal.d" -MT"SDK/rtos/osif/osif_baremetal.o" -o "SDK/rtos/osif/osif_baremetal.o" "../SDK/rtos/osif/osif_baremetal.c"
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/platform/pal/src/can/can_pal.args" -MMD -MP -MF"SDK/platform/pal/src/can/can_pal.d" -MT"SDK/platform/pal/src/can/can_pal.o" -o "SDK/platform/pal/src/can/can_pal.o" "../SDK/platform/pal/src/can/can_pal.c"
Building file: ../SDK/platform/drivers/src/wdog/wdog_hw_access.c
Building file: ../SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.c
Building file: ../SDK/platform/drivers/src/wdog/wdog_driver.c
Building file: ../SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.c
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.args" -MMD -MP -MF"SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.d" -MT"SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.o" -o "SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.o" "../SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.c"
Invoking: Standard S32DS C Compiler
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/platform/drivers/src/wdog/wdog_driver.args" -MMD -MP -MF"SDK/platform/drivers/src/wdog/wdog_driver.d" -MT"SDK/platform/drivers/src/wdog/wdog_driver.o" -o "SDK/platform/drivers/src/wdog/wdog_driver.o" "../SDK/platform/drivers/src/wdog/wdog_driver.c"
arm-none-eabi-gcc "@SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.args" -MMD -MP -MF"SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.d" -MT"SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.o" -o "SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.o" "../SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.c"
../src/driver/flash/src/flash.c:2:27: fatal error: flash_hal_Cfg.h: No such file or directory
#include "flash_hal_Cfg.h"
^
compilation terminated.
Invoking: Standard S32DS C Compiler
arm-none-eabi-gcc "@SDK/platform/drivers/src/wdog/wdog_driver.args" -MMD -MP -MF"SDK/platform/drivers/src/wdog/wdog_hw_access.d" -MT"SDK/platform/drivers/src/wdog/wdog_hw_access.o" -o "SDK/platform/drivers/src/wdog/wdog_hw_access.o" "../SDK/platform/drivers/src/wdog/wdog_hw_access.c"
Building file: ../SDK/platform/drivers/src/power/power_manager.c
make: *** [src/driver/flash/src/subdir.mk:23: src/driver/flash/src/flash.o] Error 1
make: *** Waiting for unfinished jobs....
../src/main.c:28:29: fatal error: bootloader_main.h: No such file or directory
#include "bootloader_main.h"
^
compilation terminated.
Invoking: Standard S32DS C Compiler
Finished building: ../src/driver/flash/src/flash_cfg.c
arm-none-eabi-gcc "@SDK/platform/drivers/src/power/power_manager.args" -MMD -MP -MF"SDK/platform/drivers/src/power/power_manager.d" -MT"SDK/platform/drivers/src/power/power_manager.o" -o "SDK/platform/drivers/src/power/power_manager.o" "../SDK/platform/drivers/src/power/power_manager.c"
make: *** [src/subdir.mk:20: src/main.o] Error 1

Finished building: ../SDK/rtos/osif/osif_baremetal.c

Finished building: ../SDK/platform/pal/src/can/can_pal.c

Finished building: ../SDK/platform/drivers/src/power/S32K1xx/power_manager_S32K1xx.c
Finished building: ../SDK/platform/drivers/src/wdog/wdog_driver.c
Finished building: ../SDK/platform/drivers/src/power/S32K1xx/power_smc_hw_access.c


Finished building: ../SDK/platform/drivers/src/wdog/wdog_hw_access.c


Finished building: ../SDK/platform/drivers/src/power/power_manager.c

"make -j12 all" terminated with exit code 2. Build might be incomplete.

17:05:05 Build Failed. 5 errors, 0 warnings. (took 2s.504ms)

 

0 Kudos
Reply

7,378 Views
jiri_kral
NXP Employee
NXP Employee

Hi,

 

The project is for Older S32 Design Studio for ARM v2018.R1 and is not compatible with S32DS v 3.4. Please download older S32DS. 

 

Jiri 

0 Kudos
Reply

7,318 Views
andyknitt
Contributor II

Thanks Jiri.  Unfortunately the older versions will not install on my laptop for some unknownreason.  I had been working with NXP support on that installation issue and they advised to use S32 Design Studio for S32 Platform since it's the latest product.  

0 Kudos
Reply