S32 Design Studio for ARM Version 2018.R1 for MCU FS32K116

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for ARM Version 2018.R1 for MCU FS32K116

ソリューションへジャンプ
4,276件の閲覧回数
lohrsistemas
Contributor IV

Hi team,

Can I use IDE S32 Design Studio for ARM Version 2018.R1 for MCU FS32K116 project development?

Thank you.

タグ(2)
1 解決策
3,897件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello lohrsistemas‌,

Yes the S32 Design Studio for ARM 2018.R1 supports the S32K116 device. Please ensure you install the latest update to have the best experience. S32 Design Studio for ARM 2018.R1 - Update 10 available 

Here you can see we have many example projects for the S32K116 device within the S32 SDK v3.0.0:

pastedImage_2.png

Hope it helps,

Mike

元の投稿で解決策を見る

4 返答(返信)
3,898件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello lohrsistemas‌,

Yes the S32 Design Studio for ARM 2018.R1 supports the S32K116 device. Please ensure you install the latest update to have the best experience. S32 Design Studio for ARM 2018.R1 - Update 10 available 

Here you can see we have many example projects for the S32K116 device within the S32 SDK v3.0.0:

pastedImage_2.png

Hope it helps,

Mike

3,897件の閲覧回数
lohrsistemas
Contributor IV

Hello Mike,

I'm using the S32K116_32qfn, but I only find S32K116_48lqfp in packages avaliables. Is there another upate to enable this package in Processor Expert?

Thanks for you help.

0 件の賞賛
返信
3,897件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi lohrsistemas‌,

As the Processor Expert is part of the S32 SDK, this question is specific enough to be best answered by the experts at: S32 SDK community.

They should be able to provide some answer.

Best Regards,

Mike

0 件の賞賛
返信
3,897件の閲覧回数
lohrsistemas
Contributor IV

Hi Mike,

Thanks for your help.

0 件の賞賛
返信