S32 Design Studio for ARM (Linux)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for ARM (Linux)

21,654件の閲覧回数
amitwarbhe
Contributor I

Even with admin privilege not able to install this binary on ubuntu - 22.04 with activation code - 1992-D57A-4A33-66CA.

Kindly help.

ラベル(1)
0 件の賞賛
返信
16 返答(返信)

19,688件の閲覧回数
frank_darcy
Contributor I

Do any network ports need to be open to successfully send an activation request to the remote activation server? 

0 件の賞賛
返信

19,683件の閲覧回数
frank_darcy
Contributor I

Ok, I think I can answer my own question. In S32DS_ARM_Installation_Guide.pdf I found this note...

Note: Make sure that TLS 1.2 protocol is enabled:
• Open Windows Control Panel > Network and Internet > Internet Options > Advanced >
Settings.
• In the Security section make sure the Use TLS 1.2 checkbox is checked. If not, check it and click
the Apply button.

So TLS implies it is a HTTPS request, presumably on the standard port 443? So if the machine has internet access working to https sites then the required port for license activation is open. I'm pretty sure TLS 1.2 is enabled by default on Ubuntu 22.04, but it can be checked. 
eg. https://support.messagemedia.com/hc/en-us/articles/4765182432399-How-to-check-if-you-re-TLS-1-2-comp...

0 件の賞賛
返信

21,405件の閲覧回数
amitwarbhe
Contributor I

Please provide resolution on priority, I have provided all necessary information from my end.

0 件の賞賛
返信

20,963件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

we met similar issues on few PC Machines - but no solution yet. The cause of the issue is Java SIGSEGV crash when calling license service, but we aren't able find reason why Java crashes. 

0 件の賞賛
返信

18,871件の閲覧回数
xcggg
Contributor I
Hi, I was wondering if there is any news about the solution yet. I have met the same problem on ubuntu 22.04 too. Thank you.
0 件の賞賛
返信

18,860件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

sorry, still no solution yet. 

0 件の賞賛
返信

21,390件の閲覧回数
amitwarbhe
Contributor I

Error Screenshots for installing design studio version 3.5 with activation code: A80A-6532-7AFA-413D

0 件の賞賛
返信

21,440件の閲覧回数
amitwarbhe
Contributor I

I am currently installing with activation code :   A80A-6532-7AFA-413D, can you please check and confirm the server registration from your end?

 

0 件の賞賛
返信

21,520件の閲覧回数
amitwarbhe
Contributor I

can I get the offline installer of version 3.5 with activation code:  A80A-6532-7AFA-413D

0 件の賞賛
返信

21,522件の閲覧回数
amitwarbhe
Contributor I

can I get the offline installer of version 3.5 with activation code:  A80A-6532-7AFA-413D

 

0 件の賞賛
返信

21,586件の閲覧回数
amitwarbhe
Contributor I

one of my friend is able to install with same linux version and laptop configuration

0 件の賞賛
返信

21,590件の閲覧回数
amitwarbhe
Contributor I

I have tried installing version 3.5 with this code as well A80A-6532-7AFA-413D, but no luck

0 件の賞賛
返信

21,588件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Can you please share installation log? 

0 件の賞賛
返信

21,584件の閲覧回数
amitwarbhe
Contributor I
no logs being generated, its getting stuck at 6%
0 件の賞賛
返信

21,591件の閲覧回数
amitwarbhe
Contributor I

sudo apt-get install openjdk-8-jre openjfx, this I have already done

all other linux packages which are mentioned in prerequisites

0 件の賞賛
返信

21,597件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS v2.2 for ARM is not tested with Ubuntu v22.04. It can be used with v20.04. Did you met the Linux installation requirements - especially Java version 8 (this version is not available on Ubuntu 22.04 by default)?

0 件の賞賛
返信