S32 Design Studio for ARM (Linux)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for ARM (Linux)

22,916 Views
amitwarbhe
Contributor I

Even with admin privilege not able to install this binary on ubuntu - 22.04 with activation code - 1992-D57A-4A33-66CA.

Kindly help.

Labels (1)
0 Kudos
Reply
16 Replies

20,950 Views
frank_darcy
Contributor I

Do any network ports need to be open to successfully send an activation request to the remote activation server? 

0 Kudos
Reply

20,945 Views
frank_darcy
Contributor I

Ok, I think I can answer my own question. In S32DS_ARM_Installation_Guide.pdf I found this note...

Note: Make sure that TLS 1.2 protocol is enabled:
• Open Windows Control Panel > Network and Internet > Internet Options > Advanced >
Settings.
• In the Security section make sure the Use TLS 1.2 checkbox is checked. If not, check it and click
the Apply button.

So TLS implies it is a HTTPS request, presumably on the standard port 443? So if the machine has internet access working to https sites then the required port for license activation is open. I'm pretty sure TLS 1.2 is enabled by default on Ubuntu 22.04, but it can be checked. 
eg. https://support.messagemedia.com/hc/en-us/articles/4765182432399-How-to-check-if-you-re-TLS-1-2-comp...

0 Kudos
Reply

22,667 Views
amitwarbhe
Contributor I

Please provide resolution on priority, I have provided all necessary information from my end.

0 Kudos
Reply

22,225 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

we met similar issues on few PC Machines - but no solution yet. The cause of the issue is Java SIGSEGV crash when calling license service, but we aren't able find reason why Java crashes. 

0 Kudos
Reply

20,133 Views
xcggg
Contributor I
Hi, I was wondering if there is any news about the solution yet. I have met the same problem on ubuntu 22.04 too. Thank you.
0 Kudos
Reply

20,122 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

sorry, still no solution yet. 

0 Kudos
Reply

22,652 Views
amitwarbhe
Contributor I

Error Screenshots for installing design studio version 3.5 with activation code: A80A-6532-7AFA-413D

0 Kudos
Reply

22,702 Views
amitwarbhe
Contributor I

I am currently installing with activation code :   A80A-6532-7AFA-413D, can you please check and confirm the server registration from your end?

 

0 Kudos
Reply

22,782 Views
amitwarbhe
Contributor I

can I get the offline installer of version 3.5 with activation code:  A80A-6532-7AFA-413D

0 Kudos
Reply

22,784 Views
amitwarbhe
Contributor I

can I get the offline installer of version 3.5 with activation code:  A80A-6532-7AFA-413D

 

0 Kudos
Reply

22,848 Views
amitwarbhe
Contributor I

one of my friend is able to install with same linux version and laptop configuration

0 Kudos
Reply

22,852 Views
amitwarbhe
Contributor I

I have tried installing version 3.5 with this code as well A80A-6532-7AFA-413D, but no luck

0 Kudos
Reply

22,850 Views
jiri_kral
NXP Employee
NXP Employee

Can you please share installation log? 

0 Kudos
Reply

22,846 Views
amitwarbhe
Contributor I
no logs being generated, its getting stuck at 6%
0 Kudos
Reply

22,853 Views
amitwarbhe
Contributor I

sudo apt-get install openjdk-8-jre openjfx, this I have already done

all other linux packages which are mentioned in prerequisites

0 Kudos
Reply

22,859 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS v2.2 for ARM is not tested with Ubuntu v22.04. It can be used with v20.04. Did you met the Linux installation requirements - especially Java version 8 (this version is not available on Ubuntu 22.04 by default)?

0 Kudos
Reply