S32 Design Studio for ARM 2.2 – License activation error (CLLReason errorNo=27: maximum number of re

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for ARM 2.2 – License activation error (CLLReason errorNo=27: maximum number of re

Jump to solution
2,054 Views
baikjongyoub
Contributor I

Hello,

I am having a license activation problem with S32 Design Studio for ARM v2.2 and I can no longer use the tool.

  • Product: S32 Design Studio for ARM

  • Version: 2.2

  • OS: Windows 10 (64-bit)

  • License type: Node-locked (activation code)

  • Activation Code: 3668-673A-125A-5626 

When I start S32DS, the Product Licenses window shows:

Status: License missing

If I click Activate and enter my activation code, I immediately get the following error:

CLLReason [errorNo=27, errorString=Error sending an return request to a remote activation server and processing the response. The maximum number of returns is reached, contact your product vendor if you need help. (FNP error 0), flxActMajorErrNo=0, flxActMinorErrNo=0, flxActSysErrNo=0, flxCommErrNo=0]

From what I understand, this means that the maximum number of returns/moves for this activation code has been reached.
In the past I have reinstalled S32DS and/or Windows several times, so the license might have been returned/activated many times.

I have already tried:

  • Running S32DS as Administrator

  • Checking my internet connection and firewall/proxy settings

  • Using both online activation and the “Generate offline request” option

The problem is still the same and I cannot activate the product anymore.

Could you please reset the return counter for this activation code or issue a new activation code so that I can activate S32 Design Studio for ARM 2.2 on my current PC?

I can provide any additional information (log files, screenshots, etc.) if needed.

Thank you in advance for your help.

Best regards,

jongyoub baik.

0 Kudos
Reply
1 Solution
2,024 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you should be able activate S32DS again with your old code. 

View solution in original post

0 Kudos
Reply
2 Replies
2,025 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you should be able activate S32DS again with your old code. 

0 Kudos
Reply
425 Views
tk8357
Contributor I

I'm having this same issue and I can't seem to figure out how to fix it

0 Kudos
Reply