S32 Design Studio Installation Issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio Installation Issues

2,399件の閲覧回数
deepakachiradon
Contributor II

Hello Good morning,

My name is Deepak from India. My questions are regarding Configuring IAR 8.22.1 plugins to S32 Design Studio and which is the version need to use for S32K116.

1. I am facing issues in configuring Plugins of IAR to S32 Design Studio. The version I am using is S32 Design Studio for ARM V2018 R1. The issue log I mentioned below.

Operation details:

  • Cannot complete the install because one or more required items could not be found.
    Software being installed: IAR Common Components 2.1.0.201804152231 (com.iar.common.feature.feature.group 2.1.0.201804152231)
  • Missing requirement: IAR Common UI Components 1.8.0.201804152231 (com.iar.ide.common.ui 1.8.0.201804152231) requires 'bundle org.eclipse.ui.trace 0.0.0' but it could not be found
  • Cannot satisfy dependency:
    From: IAR Common Components 2.1.0.201804152231 (com.iar.common.feature.feature.group 2.1.0.201804152231)
    To: com.iar.ide.common.ui [1.8.0.201804152231]

2. Is the version I am using for S32K116 is correct or Wrong?

 

Please help me regarding the question.

Thanks

Deepak Achar

タグ(4)
0 件の賞賛
返信
1 返信

1,843件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello Deepak,

It seems the versions of S32DS and IAR are ok.

You should be able to build the project with IAR toochain for S32K116.

But the IAR debug may not support this derivative yet.

Could you possibly check this document: HOWTO: Install IAR Eclipse plug-in into S32 Design Studio for ARM 

Please let us know if does not help you.

You should be able to 

Thanks

Stan.

0 件の賞賛
返信