RAppID BL Tools for S32K144

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RAppID BL Tools for S32K144

3,479 Views
zhaoyanling
Contributor III

Dear expert:

My development is based on S32K144 EVB –Q100. Now I meet a question on RAppID Boot Loader Utility. The version of RAppID BL tools is shown as following:

question_1.bmp

My steps are following:

1. insert openSDA USB prot, and there is a mass storage is shown on my computer:

question_2.bmp

2.I copy SK144_Bootloader.rbf into F disc:

question_3.bmp

3.the pins are configured as following:

Jumper

Configuration

Description

J104

1-2

Reset signal to OpenSDA,used to enter into OpenSDA Bootloader mode

J107

1-2

S32K144 powered by 12V power source.

4.only push the “reset” button on EVB, not power off.

5.open the “RAppID Boot Loader Utility”,and setings are shown as following:

question_4.bmp

6.but the error is shown as following:

question_5.bmp

7.I have tried some different rbf file, but the error is always the same. These rbf files are attached.

 Could you help me? my questions are:

1. Is the step 4 right? Should I power off the EVB after copy rbf file into mass storage device?

2.Need I copy *.rbm or rba file into the mass storage device?

3. how can I get the correct rbf file?

Thank you very much for your kind help!

0 Kudos
Reply
2 Replies

3,254 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

there is timeout for boot loader. Just reset your board and try connection again. The rbf file can be also flashed in s32ds - it is nornmal s-record file. But copy it in mass storage should work okay. 

Jiri 

0 Kudos
Reply

2,805 Views
markus_29
Contributor II

Hi,

how to flash the rbl file with the S32DS to a S32K148?

Markus

0 Kudos
Reply