Processor Expert Component Inspector view is blank, Components View cannot be shown

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Processor Expert Component Inspector view is blank, Components View cannot be shown

Jump to solution
2,668 Views
rsating
Contributor III

The Processor Expert "Components Inspector" view is blank for my project, see screenshot below. Also, the "Components" view refuses to display.  Could it be due to the "Peripheral is already used" error?

S32DS_component-inspector-empty.png

Below is the menu sequence used in attempting to display the "Components" view:

S32DS_show-view_components.png

Why does the view not open?  How can we troubleshoot the errors without it?  I may have added components more than once, but I cannot see a way to investigate or resolve the problem. Can you help us understand how this works?

Attached is the S32DS project, in case it helps.

Thanks

0 Kudos
Reply
1 Solution
2,656 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

this example is for older SDK version which is not supported by S32DS for ARN v2.2. Try to open it with S32DS for ARM 2018.R1

 

Jiri 

View solution in original post

0 Kudos
Reply
1 Reply
2,656 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

this example is for older SDK version which is not supported by S32DS for ARN v2.2. Try to open it with S32DS for ARM 2018.R1

 

Jiri 

0 Kudos
Reply