Problem with Clock_Ip_TriggerUpdateCgmXDivTrigCtrlTctlHhenUpdStat os S32K312

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with Clock_Ip_TriggerUpdateCgmXDivTrigCtrlTctlHhenUpdStat os S32K312

ソリューションへジャンプ
8,499件の閲覧回数
jacopo_costella
Contributor II

Hello,

with S32DS Ver. 3.4, after running pin and clock configuration of  S32K312, I tested a simple program and when entering the function:

Clock_Ip_TriggerUpdateCgmXDivTrigCtrlTctlHhenUpdStat (file Clock_Ip_DividerTrigger.c)

the debug session crashed ehwn executing the instruction

DividerStatus = Clock_Ip_apxCgm[Instance][SelectorIndex]->MUX_DIV_UPD_STAT & MC_CGM_MUX_DIV_UPD_STAT_DIV_STAT_MASK;

 

Instance = 0;

SelectorIndex = 0.

Do you have any idea?

 

Thank you very much,

Jacopo

 

 

 

0 件の賞賛
返信
1 解決策
8,466件の閲覧回数
jacopo_costella
Contributor II

Hello Daniel,

thank you very much for your fast feedback. I noticed your suyggestion here;

https://community.nxp.com/t5/S32K/How-to-compile-S32K3-HSE-FW-in-project/m-p/1541925#M18475https://c...

 

which demo were you referring to?

Regards,

Jacopo

 

 

 

 

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
8,447件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @jacopo_costella,

Currently, we have some issues with our system, and the demo can't be located at nxp.com.

We are working on it.

All the HSE_FW documentation can be found in the Secure files under an NDA on the S32K3xx webpage though:

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32k-auto-gener...

I understand the HSE_FW hasn't been installed on the MCU yet.

Can you share the project so that I can test it?

 

Thank you,

BR, Daniel

 

 

0 件の賞賛
返信
8,440件の閲覧回数
jacopo_costella
Contributor II

Hello Daniel,

 

thank you for your reply.

 

Please find attached the project.

 

Have a nice day,

 

Jacopo

0 件の賞賛
返信
8,434件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Jacopo,

I don't have this old RTD version installed, so I can't modify and recompile the project.

Anyway, the clock configuration is not correct.

Please set all the clock as per the RM, Table 148. Option B - Reduced Speed mode (CORE_CLK @ 120 MHz).

This is just an example from Clocking use case examples (RM, Section 24.7.2).
However, any clock frequency selected must adhere to the same clock divider ratios shown in Clocking use case examples.

Otherwise, we can't guarantee the specified functionality of the MCU.

 

Regards,

Daniel

 

 

0 件の賞賛
返信
8,399件の閲覧回数
jacopo_costella
Contributor II

Hello Daniel,

How did you check the incorrect core clock value? From the tool it is set to 120 MHz. 

Regards,

Jacopo

0 件の賞賛
返信
8,396件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

All the clocks must be set according to the table (including the PLL clock), or at least the ratios between the clocks must be maintained.

 

Regards,

Daniel

0 件の賞賛
返信
8,387件の閲覧回数
jacopo_costella
Contributor II

Hello Daniel,

problem fixed. Thank you very much,

Jacopo

 

0 件の賞賛
返信
8,470件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @jacopo_costella,

Is the HSE_FW installed?

 

Thanks,

BR, Daniel

0 件の賞賛
返信
8,467件の閲覧回数
jacopo_costella
Contributor II

Hello Daniel,

thank you very much for your fast feedback. I noticed your suyggestion here;

https://community.nxp.com/t5/S32K/How-to-compile-S32K3-HSE-FW-in-project/m-p/1541925#M18475https://c...

 

which demo were you referring to?

Regards,

Jacopo

 

 

 

 

 

 

 

0 件の賞賛
返信