Package installation issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Package installation issue

Jump to solution
4,341 Views
Silvano
Contributor I

Hello all,

I would like to program a S32K396 MCU to drive a motor.

When I plug the MCU to the computer and try to create a new S32DS Application Project , I face this issue :

Silvano_1-1708432113929.png

 

To solve this problem, I tried to install " SW32K3_S32DS_3.4.1_D2108.zip " which is the package for S32K3 devices.

However, when I go on the "S32DS Extensions and Updates" section, I see that this package is not installed : 

Silvano_2-1708432275818.png

Silvano_3-1708432300175.png

 

When I try to install it, I face this issue : -

Silvano_4-1708432356007.png

 

Even when I select all 6 items, I can't install : 

Silvano_5-1708432481151.png

 

I also tried to click on help > Install new software > work with "All Available Sites" . Then first I got these errors : 

Silvano_6-1708432696723.png

Then : 

Silvano_7-1708432718390.png

 

Silvano_8-1708432727407.png

 

And finally after clicking "next", this problem occured : 

Silvano_9-1708432760548.png

 

In conclusion I still can't create a new project to start program the S32K39 MCU.

I also don't have "Project from Example" except M0plus.

 

Can you please help me to solve this problem ?

 

 

 

 

 

0 Kudos
Reply
1 Solution
4,148 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Silvano 

The example code provided with the RTDs can be found by creating a project from an example. Check the following links, It has information related to this topic. 

HOWTO: S32 Design Studio - Create a New S32DS Project from Example

View solution in original post

0 Kudos
Reply
11 Replies
4,310 Views
Silvano
Contributor I

Thank you.

I installed the S32DS 3.5 but I still have this issue when I try to install "New software"

Silvano_0-1708504901056.png

And the "Extensions and Updates" section doesn't show the installed packages :

Silvano_1-1708505789464.png

Silvano_3-1708505852653.png

 

Silvano_2-1708505833887.png

 

Finally, I still don't have example projects to start programming the S32K396

 

0 Kudos
Reply
4,300 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Silvano 

The cause is probably due to a lack of the required dependency in the S32 Design Studio package you are trying to install. Could you share the names of the packages you are looking to install?

0 Kudos
Reply
4,269 Views
Silvano
Contributor I

I am trying to install these packages : "S32 Design Studio S32 SDK" , "S32 Design Studio S32K396 SDK"  and "S32 Design Studio S32K396.P01 SDK".

But for any package I tried to install, I have the same error : 

Silvano_0-1708590305679.png

 

Is there any number I can call ? I have this issue for a week and it is starting to become an emergency.

Thank you.

0 Kudos
Reply
4,234 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Silvano 

Please check if S32DS Extensions and Updates -> Manage Sites, you have the following: 

VaneB_0-1708629464210.png

For S32K96 devices, the available software can be found through S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M. To install these packages is required the installation of the S32K396 development package, which can be found at the previous share link at the Automotive SW - S32K3 - S32 Design Studio. 

Also, could you please share your installation details? This can be found at S32DS Extensions and Updates. 

 

0 Kudos
Reply
4,216 Views
Silvano
Contributor I

Hi @VaneB 

My installation details are : 

Silvano_0-1708684496433.png

Silvano_1-1708684510972.png

 

I did as you said, I installed " SW32K39x_S32DS_3.5.6_D2309.zip " before the installation of "Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M " packages . However when I try to install "S32 Design Studio S32K396 development package 1.0.0.6797AcJMj4F773793K7K55CK" I still have this error : 

<<Cannot complete the install because of a conflicting dependency.
Software being installed: S32K396 development package 3.5.6.202309291159 (com.nxp.s32ds.s32k396.dev.feature.feature.group 3.5.6.202309291159)
Software currently installed: S32 Design Studio Tools 3.5.0.202207261752 (com.nxp.s32ds.platform.ide.tools.feature.feature.group 3.5.0.202207261752)
Only one of the following can be installed at once:
com.nxp.s32ds.platform.ide.tools.feature_root 3.5.8.202311282316
com.nxp.s32ds.platform.ide.tools.feature_root 3.5.0.202207261752
com.nxp.s32ds.platform.ide.tools.feature_root 3.5.10.202401301332
com.nxp.s32ds.platform.ide.tools.feature_root 3.5.6.202309290941
Cannot satisfy dependency:
From: S32 Design Studio Tools 3.5.0.202207261752 (com.nxp.s32ds.platform.ide.tools.feature.feature.group 3.5.0.202207261752)
To: org.eclipse.equinox.p2.iu; com.nxp.s32ds.platform.ide.tools.feature_root [3.5.0.202207261752,3.5.0.202207261752]
Cannot satisfy dependency:
From: S32 Design Studio for S32 Platform Tools 3.5.10.202401301332 (com.nxp.s32ds.platform.ide.tools.feature.feature.group 3.5.10.202401301332)
To: org.eclipse.equinox.p2.iu; com.nxp.s32ds.platform.ide.tools.feature_root [3.5.10.202401301332,3.5.10.202401301332]
Cannot satisfy dependency:
From: S32 Design Studio for S32 Platform Tools 3.5.6.202309290941 (com.nxp.s32ds.platform.ide.tools.feature.feature.group 3.5.6.202309290941)
To: org.eclipse.equinox.p2.iu; com.nxp.s32ds.platform.ide.tools.feature_root [3.5.6.202309290941,3.5.6.202309290941]
Cannot satisfy dependency:
From: S32 Design Studio for S32 Platform Tools 3.5.8.202311282316 (com.nxp.s32ds.platform.ide.tools.feature.feature.group 3.5.8.202311282316)
To: org.eclipse.equinox.p2.iu; com.nxp.s32ds.platform.ide.tools.feature_root [3.5.8.202311282316,3.5.8.202311282316]
Cannot satisfy dependency:
From: S32K396 development package 3.5.6.202309291159 (com.nxp.s32ds.s32k396.dev.feature.feature.group 3.5.6.202309291159)
To: org.eclipse.equinox.p2.iu; com.nxp.s32ds.platform.ide.tools.feature.feature.group 3.5.6 >>

 

Silvano_2-1708684739545.png

Silvano_3-1708684848680.png

 

 

0 Kudos
Reply
4,164 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Silvano 

I have reviewed your installation details and I have noticed that you missed the installation of some packages required for the S32K396 software installation. In the following image, I have highlighted the relevant packages. 

VaneB_0-1708939894380.png

Also, regarding the latest images, you need to select all the packages shown in the window. For reference, I am attaching the packages I have installed.

VaneB_1-1708940343642.png

VaneB_2-1708940362480.png

 

 

0 Kudos
Reply
4,155 Views
Silvano
Contributor I

Hi @VaneB 

 

I finally managed to solve the problem. Thank you.

 

I have a last question, where can I find PWM code examples for S32K396 ?

 

0 Kudos
Reply
4,149 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Silvano 

The example code provided with the RTDs can be found by creating a project from an example. Check the following links, It has information related to this topic. 

HOWTO: S32 Design Studio - Create a New S32DS Project from Example

0 Kudos
Reply
4,146 Views
Silvano
Contributor I
ok thank you for your help!
0 Kudos
Reply
4,258 Views
Silvano
Contributor I
I also have the issue "Launch failed. Binary not found." when I run a C file.
0 Kudos
Reply
4,321 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Silvano 

S32K396 devices are just supported by S32DS 3.5. Please download this IDE version and the corresponding package. 

Also, if you have doubts about which version of the tools supports the various packages of the S32K3 devices, please consult the release notes of each package.

 

B.R.

VaneB

0 Kudos
Reply