NXP Eclipse plug-ins for freertos

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP Eclipse plug-ins for freertos

ソリューションへジャンプ
7,261件の閲覧回数
prashantsathe
Contributor III

Hi,

 

"S32DS: S32 Design Studio IDE" feature state that it has eclipse plug in support for freertos  like below

 

                 "Support for additional downloadable NXP Eclipse plug-ins including RTOS-awareness (such as FreeRTOS,  

                   Core  self test)"

 

Could you please tell me procedure to do so..

 

-Prahshant

ラベル(1)
0 件の賞賛
返信
1 解決策
6,156件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

Regarding FreeRTOS - there has been recently added Kernel awareness into S32DS for ARM v1.2/ Power v1.1.

You can enable this feature in the Debug Configuration dialog -> OS Awareness Tab:

pastedImage_0.png

There is also FreeRTOS port for the S32K is available as part of S32K SDK (which is part of S32DS for ARM v1.2 [Windows] installer)

You can try to build and debug the FreeRTOS example available  (File -> New S32DS Project from... -> FreeRTOS_Example):

pastedImage_1.png

pastedImage_3.png

Hope it helps.

Stan.

元の投稿で解決策を見る

7 返答(返信)
6,157件の閲覧回数
stanish
NXP Employee
NXP Employee

Hello,

Regarding FreeRTOS - there has been recently added Kernel awareness into S32DS for ARM v1.2/ Power v1.1.

You can enable this feature in the Debug Configuration dialog -> OS Awareness Tab:

pastedImage_0.png

There is also FreeRTOS port for the S32K is available as part of S32K SDK (which is part of S32DS for ARM v1.2 [Windows] installer)

You can try to build and debug the FreeRTOS example available  (File -> New S32DS Project from... -> FreeRTOS_Example):

pastedImage_1.png

pastedImage_3.png

Hope it helps.

Stan.

6,155件の閲覧回数
bix010
Contributor III

Hi,

I tried doing this, but when stepping through my code, the OS Details Browser is blank, and OS Resources shows "OS resources are not available using your target and GDB". I'm using FreeRTOS on the DEVKIT-MPC5748G.

Appreciate any help!

0 件の賞賛
返信
6,156件の閲覧回数
ziomocci
Contributor IV

Hi Stan,

 I am following the tutorial, but when I try to build the example unfortunately I find few problems as depicted in the screenshot.

Cattura.PNG

It seems, very strange, that the requested headers are not present.

I am using this version of S32DS

Cattura1.PNG

Any suggestion would be very appreciated,

B.R.

Andrea Mocci

0 件の賞賛
返信
6,156件の閲覧回数
edgarmichel
Contributor II

Hello Andrea,
would you please give me some details what you did?
When open the RTOS example there are no freeRTOS files available.
I am using SDK on Linux, Version 2 update3

Thanks Edgar

0 件の賞賛
返信
6,156件の閲覧回数
ziomocci
Contributor IV

Hello Edgar,

 To be honest we have left the FreeRTOS solution, moreover I was working on Windows 7 platform.

Have you tried to install everything once time again? 

AM

0 件の賞賛
返信
6,156件の閲覧回数
ziomocci
Contributor IV

Problem solved Stan!!!

I have not noticed that Processor Expert configuration shall be build before!!! 

Consider the problem closed (for now at least :smileyhappy: )

B.R.

Andrea

0 件の賞賛
返信
6,156件の閲覧回数
prashantsathe
Contributor III

Thanks , Appreciated.

0 件の賞賛
返信