NEED SPI working api to read and write for s32 design studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NEED SPI working api to read and write for s32 design studio

跳至解决方案
1,033 次查看
selvarajasekar
Contributor III


"I'm currently utilizing S32 Design Studio 3.4 for development, focusing on the S32K312 microcontroller. In my project, I'm using the example code for SPI, specifically the lpspi_flexio_ip_transfer_s32k312 which is a loopback example. I require documentation on the SPI API keys for both read and write operations."


"I require functional APIs to execute both write and read operations over the  SPI interface."
I require documentation or working SPI code for s32k312.

0 项奖励
回复
1 解答
1,006 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @selvarajasekar,

All available RTD documentation can be found in the installation folder of the RTD.

 

Regards,

Daniel

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,007 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @selvarajasekar,

All available RTD documentation can be found in the installation folder of the RTD.

 

Regards,

Daniel

0 项奖励
回复