The project BSP Z4 1 was created for Kinetis SDK SDK S32 PA 15 which is not
installed in this product (repository SDK S32 PA 15 not found). lt is
recommended to skip loading and install Kinetis SDK SDK S32 PA 15 first
(located in "(KSDK)/tools/eclipse update").
f you continue loading, Processor Expert automatically converts configuration
to use currently installed components. Such project might not work.
上面是报的错误,我自始至终一直使用的最新的各种安装包,如何解决??
Hi,
please make sure that you are using S32DS for Power Architecture v2.1 and have installed S32 SDK v3.0.3:
i am using S32DS for Power Architecture v2.1 and i have installed S32 SDK v3.0.3 but still have same problem.