NEED SPI working api to read and write for s32 design studio

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NEED SPI working api to read and write for s32 design studio

Jump to solution
1,029 Views
selvarajasekar
Contributor III


"I'm currently utilizing S32 Design Studio 3.4 for development, focusing on the S32K312 microcontroller. In my project, I'm using the example code for SPI, specifically the lpspi_flexio_ip_transfer_s32k312 which is a loopback example. I require documentation on the SPI API keys for both read and write operations."


"I require functional APIs to execute both write and read operations over the  SPI interface."
I require documentation or working SPI code for s32k312.

0 Kudos
Reply
1 Solution
1,002 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @selvarajasekar,

All available RTD documentation can be found in the installation folder of the RTD.

 

Regards,

Daniel

View solution in original post

0 Kudos
Reply
1 Reply
1,003 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @selvarajasekar,

All available RTD documentation can be found in the installation folder of the RTD.

 

Regards,

Daniel

0 Kudos
Reply