NEED SPI working api to read and write for s32 design studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NEED SPI working api to read and write for s32 design studio

ソリューションへジャンプ
911件の閲覧回数
selvarajasekar
Contributor III


"I'm currently utilizing S32 Design Studio 3.4 for development, focusing on the S32K312 microcontroller. In my project, I'm using the example code for SPI, specifically the lpspi_flexio_ip_transfer_s32k312 which is a loopback example. I require documentation on the SPI API keys for both read and write operations."


"I require functional APIs to execute both write and read operations over the  SPI interface."
I require documentation or working SPI code for s32k312.

0 件の賞賛
返信
1 解決策
884件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @selvarajasekar,

All available RTD documentation can be found in the installation folder of the RTD.

 

Regards,

Daniel

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
885件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @selvarajasekar,

All available RTD documentation can be found in the installation folder of the RTD.

 

Regards,

Daniel

0 件の賞賛
返信