Missing requirement for S32k3xx RTD extension

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Missing requirement for S32k3xx RTD extension

ソリューションへジャンプ
1,742件の閲覧回数
mnmurill
Contributor I

I have installed the S32 design studio v 3.5 to work with SK32K312 microcontroller and need to install the extension/update of S32k3xx RTC v3.0.0

mnmurill_0-1729690655172.png

The installation seems to proceed but it is not successful the Reason shown is that there is a missing requirement, but I don't know how to get that requirement.

mnmurill_1-1729690715214.png

 

 

タグ(1)
0 件の賞賛
返信
1 解決策
1,680件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

S32K3 Standard Software -> Automotive SW - S32K3 - S32 Design Studio

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
1,673件の閲覧回数
mnmurill
Contributor I

Thank you for the support, using the 1st comment link (instructions) and the last comment link (files to download) I managed to complete the installation of the set up required. 

0 件の賞賛
返信
1,717件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please offline install it by refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
1,698件の閲覧回数
mnmurill
Contributor I

Hi, thanks for the answer I followed the instructions but in step 3 clicking in any of it links redirects me to my NXP profile. Any other way to download the S32k3xx RTD extension?

0 件の賞賛
返信
1,692件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

You must be logged into your account on NXP.com to gain access to the download link.

0 件の賞賛
返信
1,685件の閲覧回数
mnmurill
Contributor I

Hi, thank you for your answer. I am logged (see figure below) but when I click on the links of step 3 it redirects me to my profile page in nxp.

mnmurill_0-1729754472565.png

 

0 件の賞賛
返信
1,681件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

S32K3 Standard Software -> Automotive SW - S32K3 - S32 Design Studio

0 件の賞賛
返信