Missing requirement for S32k3xx RTD extension

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing requirement for S32k3xx RTD extension

Jump to solution
1,747 Views
mnmurill
Contributor I

I have installed the S32 design studio v 3.5 to work with SK32K312 microcontroller and need to install the extension/update of S32k3xx RTC v3.0.0

mnmurill_0-1729690655172.png

The installation seems to proceed but it is not successful the Reason shown is that there is a missing requirement, but I don't know how to get that requirement.

mnmurill_1-1729690715214.png

 

 

0 Kudos
Reply
1 Solution
1,685 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

S32K3 Standard Software -> Automotive SW - S32K3 - S32 Design Studio

View solution in original post

0 Kudos
Reply
6 Replies
1,678 Views
mnmurill
Contributor I

Thank you for the support, using the 1st comment link (instructions) and the last comment link (files to download) I managed to complete the installation of the set up required. 

0 Kudos
Reply
1,722 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please offline install it by refer to HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
1,703 Views
mnmurill
Contributor I

Hi, thanks for the answer I followed the instructions but in step 3 clicking in any of it links redirects me to my NXP profile. Any other way to download the S32k3xx RTD extension?

0 Kudos
Reply
1,697 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

You must be logged into your account on NXP.com to gain access to the download link.

0 Kudos
Reply
1,690 Views
mnmurill
Contributor I

Hi, thank you for your answer. I am logged (see figure below) but when I click on the links of step 3 it redirects me to my profile page in nxp.

mnmurill_0-1729754472565.png

 

0 Kudos
Reply
1,686 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

S32K3 Standard Software -> Automotive SW - S32K3 - S32 Design Studio

0 Kudos
Reply