Make Error for CSI source in VSDK_1.1.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Make Error for CSI source in VSDK_1.1.1

1,164 次查看
hemansinghtchau
Contributor I

The make for the available library kernel source code like CSI is giving error as below: 

Error.JPG

What exactly needs to be defined to resolve the above error in the Makefile?

The details for the setup are:

VSDK: S32V234 vsdk RTM 1.1.1

Tool: MSYS

0 项奖励
回复
1 回复

1,081 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

this variable should point into s32v234 kernel sources (more details on VisionSDK_UserGuide.pdf - located in s32v234_sdk/docs/vsdk). Sources are not part of VSDK installation. 

Anyway - there are already binary kernel modules present in VSDK. To build them makes sense only if you are doing some changes. 

Jiri

0 项奖励
回复