Machine check exceptions in MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Machine check exceptions in MPC5748G

Jump to solution
26,155 Views
villevallinder
Contributor II


Hi everybody!

 

Now and then I encounter situations where a machine check exception results in the program getting stuck in IVOR1_Vector which has no implementation.

I would very much like to be able to analyze the exception information to track down the reason why this is happening.

 

More specifically I would like to know:

1) I can't seem to find the exception registers (MCSR in particular) in the register lists, are they at all available to be read in Design Studio?

2) Is there some sort of example code that actually does something, that can replace the default IVOR1_Vector loop?

 

Any information and tips would be highly appreciated.

 

Best Regards

Ville

Labels (1)
1 Solution
22,847 Views
martin_kovar
NXP Employee
NXP Employee

Hi Ville,

1) Yes, you are correct, MSCR is not in register list. But there is a workaround you can use. While debugging, click on Display selected console icon and choose powerpc-eabivle-gdb and write to the console command monitor spr 572t.

pastedImage_0.png

MCSR is marked as special purpose register 572.

2) Look at the example in the attachment. This simple example shows, how to create your own IVOR1 handler. Also you can look at the following example, which is created  for GHS and also shows, how to create IVOR1 handler.

Example MPC5777C-1b+2b_RAM_ECC_error_injection GHS614

If you have any other question, please feel free to write me back.

Regards,

Martin

View solution in original post

21 Replies
22,848 Views
martin_kovar
NXP Employee
NXP Employee

Hi Ville,

1) Yes, you are correct, MSCR is not in register list. But there is a workaround you can use. While debugging, click on Display selected console icon and choose powerpc-eabivle-gdb and write to the console command monitor spr 572t.

pastedImage_0.png

MCSR is marked as special purpose register 572.

2) Look at the example in the attachment. This simple example shows, how to create your own IVOR1 handler. Also you can look at the following example, which is created  for GHS and also shows, how to create IVOR1 handler.

Example MPC5777C-1b+2b_RAM_ECC_error_injection GHS614

If you have any other question, please feel free to write me back.

Regards,

Martin

22,574 Views
ruudsiebierski
Contributor III

To view all registers of the MCU, including the ESR registers you could also use the "All registers" debug view.

Window --> Show View --> Other...

pastedImage_1.png

pastedImage_2.png

using S32DS 2017.R1

0 Kudos
Reply
22,591 Views
huqiang
Contributor IV

Hi , Martin

        Your project "MPC5748G-IVOR1_ExceptionHandler-S32DS "is really helpful. But would you give me an example about how to get out of the "IVOR1_Exception_Handler" ,and back to the "int main(void)"  again? My project is on the MPC5748G.

Thanks,

Qiang

0 Kudos
Reply
22,591 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I have created new example for you, because I found an error in previous example I had shared here. In the previous example, IVOR1 is not caused by SMPU, but by reading uninitialized SRAM. New example shows, how to handle IVOR2 exception cause by SMPU. Please look and carefully read my comments into the example.

If you have any question about the example, please write me back.

Regards,

Martin

0 Kudos
Reply
22,579 Views
2548903578
Contributor III

Hi,

I have a similar problem.

MPC574XX uSDHC_DriverIRQHandler () 

MPC5746C ADC problem 

These two connections are the problems I raised, but there is no good solution, please give me a look

0 Kudos
Reply
22,589 Views
huqiang
Contributor IV

Hi, Martin

      I have run you IVOR2_Exception project on my MPC5748G EVB. But it seems it will cause a IVOR1 error.

Capture.PNG

      When I suspend the project, it will became as the figure shows. I try to add a breakpoint in the function of IVOR2_Exception_Handler, but it seems that the project didn't run into the IVOR2_Exception_Handler .

Is there something that I misunderstanding?

Qiang

0 Kudos
Reply
22,590 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I did not test the project via PEMicro debugger. I used Lauterbach and it works correct. I will try it on Monday and will write you back.

Regards,

Martin

22,590 Views
huqiang
Contributor IV

Hi, Martin

Thanks for your help!

Regards,

Qiang

0 Kudos
Reply
22,590 Views
martin_kovar
NXP Employee
NXP Employee

Hi,

I found the issue. If you step the code, IVOR2 occurs, but if you run the code, IVOR1 occurs. I am not sure, why this behavior becomes, but it could be possibly cause by some synchronization. Please give me a time, I will update the example.

Regards,

Martin

0 Kudos
Reply
22,590 Views
huqiang
Contributor IV

Hi, Martin

Thank you for your help.

Besides, I have a question about the register SMPU.RGDn. For example , UTest use the SMPU_0.RGD[0], BAF use the SMPU_0.RGD[1], HSM code use the SMPU_0.RGD[2]...When config the SRAM(768kB-4kB), use the SMPU_1.RGD[0],when config the SRAM(last 4kB), use the SMPU_1.RGD[1]. 

I know when to choose SMPU_0 or SMPU_1, but how about the "n" for RGD[n]?  I can not  found any information in the reference manual. Does it matter if the "n" have different value?

Regards,

Qiang

0 Kudos
Reply
22,590 Views
martin_kovar
NXP Employee
NXP Employee

Hi Qiang,

I updated the example, please see the attachment.

About your SMPU question, there are 16 descriptors for every SMPU you can use. It is not defined, which descriptor you have to use, you can choose anyone.

Regards,

Martin

22,590 Views
lakshmikanth
Contributor III

Hi Martin, 

Thanks for the whole information. I need small clarification is possible:

a) Statement (in MPC5777CRM.pdf says) : When a master tried to access the address space that is restricted for it by MPU Region descriptor, the MPU generates "PROTECTION_ERROR". 

b) So, can I assume that this "PROTECTION_ERROR" generation is nothing but updating the EARn, EDRn registers of MPU. 

c) Also, assume the MACHINE_CHECK exception is triggered by the MASTER that tried to access the mem_address not that is protected from it. So, there is no MPU intervention in generating the MACHINE CHECK exception. 

So please let me know on this if possible. Eager to here from you. 

Thank you in advance. 

0 Kudos
Reply
22,590 Views
yulianmatev
Contributor III

Hello Martin,

Your example is very helpful for me, but there is something which I do not understand. Your IVORx_Handlers always start with following code:

IVOR4_Handler:
prologue:
    e_stwu r1,-0x50 (r1) # Create stack frame and store back chain

My question is: What is the value loaded inside r1 before the execution of e_stwu ?

Where can I find some additional information regarding the values loaded inside register r0-r31 when interrupt service routine is called?

Best regards,

Yulian

0 Kudos
Reply
22,581 Views
martin_kovar
NXP Employee
NXP Employee

Hello Yulian,

r1 is used as a stack pointer. Before interrupt is executed, it is necessary to save same register values and it is necessary to create stack frame for the values. So the value stored in r1 is current top of the stack address.

Please see the document in the attachment. There are some useful information about registers.

If you have any other questions, please feel free to write me back.

Regards,

Martin

22,581 Views
huqiang
Contributor IV

Hi, Martin

Sorry to interrupt you.

I add a breakpoint in IVOR1_Exception_Handler, the project would stop into it when running the code.

But if I add a breakpoint in IVOR2_Exception_Handler, the project would not stop when running the code.

So it seems the IVOR1_Exception (machine check) would happen while IVOR2_Exception (data storage) did not happen?

You said that "IVOR1 is not caused by SMPU, but by reading uninitialized SRAM."

I got a little puzzled.

I use the SMPU module to set last 4kB read only for M0(Z4a). And then I write  the one the last 4kB.

And then the IVOR1 happened while the IVOR2 not.

I also run the code " i = *(unsigned int *)0x400bf000; *(unsigned int *)0x400bf000 = 0xAABBCCDD; " without setting any SMPU.  It would run normally.

Then I thought IVOR1 was caused by SMPU.

Can you help me to understand those codes?

Thanks!

Regards,

Qiang

0 Kudos
Reply
22,581 Views
martin_kovar
NXP Employee
NXP Employee

Hi Qiang,

sorry for that confusion.

I shared here example called MPC5748G-IVOR1_ExceptionHandler-S32DS.zip. In this example I have incorrectly initialized RAM (only 256KB from 768KB is initialize - look at the linker file). But SMPU is configured to protect last 4KB (764KB-768KB). So in this case there the problem is on the line i = *(unsigned int *)0x400bf000; because I read RAM, which is not initialized, ECC problem could happen and it causes IVOR1 exception (but it can behave randomly).

So I created second example and there is the problem which I describe above. IVOR2 occurs when you single step over this line: *(unsigned int *)0x400bf000 = 0xAABBCCDD; and IVOR1 occurs when you do not single step.

Obviously writing to protected area can create IVOR1 and also IVOR2 exception. I am not sure, why it behaves this way, but it could be caused because of synchronization (I will study this problem later).

So the behavior you describe is correct. You should get IVOR1 exception when you do not single step asm code on line *(unsigned int *)0x400bf000 = 0xAABBCCDD.

I hope I clarified it a little bit. If you have any other question, please feel free to write me back.

Regards,

Martin

0 Kudos
Reply
22,581 Views
huqiang
Contributor IV

Hi, Martin

Your reply helps me a lot.  mem.id is different between two example.

Thanks you!

Infact, I could not have IVOR2  occurs  both in "step into (F5)" mode and "resume" mode with S32 Design Studio.

All have IVOR1 occurs.

Maybe I have something configurations different from you. I am not quite sure.

I will try to find what's wrong with me tomorrow.

Thank you for your help!

Regards,

Qiang

0 Kudos
Reply
22,581 Views
martin_kovar
NXP Employee
NXP Employee

Hi Qiang,

I am also not able to get IVOR2 exception using PEMicro and S32DS Debugger. This occurs only if I use Lauterbach debugger and because I use only Lauterbach when I write examples, I thought SMPU generates IVOR2 (what a mistake :-)).

So I think you do not have to look for the mistake, because there is not any one. But this example can show you, how to handle IVOR2 (it is little bit different than IVOR1), when you will need it.

Regards,

Martin

0 Kudos
Reply
22,581 Views
huqiang
Contributor IV

Hi, Martin

Your IVOR1 and IVOR2 examples are helpful for me.

Thanks!

Regards,

Qiang

0 Kudos
Reply
22,582 Views
huqiang
Contributor IV

Hi, Martin

It works well now.

Thank you for your help!

Regards,

Qiang

0 Kudos
Reply