KEA128 UART Interrupt example code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KEA128 UART Interrupt example code

2,391 Views
emb02
Contributor V

Dear Community,

I want to test UART of FRDM-KEAZ128Q80 using UART Interrupt. But I'm not able to find any example code of UART using interrupts in S32 Design Studio for ARM for KEA128. So can you provide me Example code of UART using interrupts? 

 

I'm using,

S32 Design Studio for ARM

Version: 2.2
Build id: 200116

0 Kudos
Reply
1 Reply

2,356 Views
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello emb02_jtronix

 

Unfortunately, we don't have a specific example for this device however, you can refer to the SDK  uart_interrupt example of the Kinetis KE04 since the UART modules of KE04 and KEA128 are very similar.

Let me know if this is helpful, if you have more questions do not hesitate to ask me.
Best regards,
Omar

0 Kudos
Reply