[S32DS.3.4]Can't find SDK from S32DS.3.4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[S32DS.3.4]Can't find SDK from S32DS.3.4

ソリューションへジャンプ
6,810件の閲覧回数
Lambert
NXP Employee
NXP Employee

HI Team,

I installed S32DS.3.4 on D:\NXP.  and 

I installed S32_SDK_BETA_0.9.0 on D:\NXP.

But S32DS.3.4 can't find this SDK when running 'Create a New Application Project', Pls check screencap as attached.

any  comment?

 

Thanks,

Lambert

0 件の賞賛
返信
1 解決策
6,760件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi @Lambert ,

To install the SDK integrated into S32DS, you must use the SDK file which contains '...updatesite.zip' in the name. Otherwise, you would need to manually add the SDK to projects individually in S32DS and the built-in integration support would not be present.

The SDK is released in 2 forms: as standalone version (filename ends with .exe), and in DS integration version (filename has ...updatesite.zip). If the DS integration version is not available, please contact the SDK team for more information.

Hope that helps,

Mike

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
6,761件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hi @Lambert ,

To install the SDK integrated into S32DS, you must use the SDK file which contains '...updatesite.zip' in the name. Otherwise, you would need to manually add the SDK to projects individually in S32DS and the built-in integration support would not be present.

The SDK is released in 2 forms: as standalone version (filename ends with .exe), and in DS integration version (filename has ...updatesite.zip). If the DS integration version is not available, please contact the SDK team for more information.

Hope that helps,

Mike

0 件の賞賛
返信
6,784件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi Lambert, 

 

which toolchain you selected when you created new project? 

jiri_kral_0-1612972280497.png

 

Jiri

0 件の賞賛
返信