Indexer Problem in S32DS for Power V1.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Indexer Problem in S32DS for Power V1.2

1,339 Views
建浩章
Contributor I

I  have created a new project in S32DS for Power V1.2, and the project is always in the index. I waited for a long time, then the index progress bar was still 0, and at this time, the S32DS running very slowly. If you has encountered this problem and solved it, please leave a message, thank you very muchProblem.png

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,222 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

It is possible for you switch from S32DS for Power v1.2 to S32DS Power 2017.R1? 

We were facing similar issue for couple customers when Network connection was active - really slow IDE and build. But this issue was caused by some firewall settings on Customer side. You can try remove network cable and see if it helps. 

Jiri

0 Kudos
Reply

1,222 Views
建浩章
Contributor I

   Thanks for your reply. I tried the method you recommended, but it didn’t work. Anyway, thank you very much.

0 Kudos
Reply