Indexer Problem in S32DS for Power V1.2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Indexer Problem in S32DS for Power V1.2

1,963件の閲覧回数
建浩章
Contributor I

I  have created a new project in S32DS for Power V1.2, and the project is always in the index. I waited for a long time, then the index progress bar was still 0, and at this time, the S32DS running very slowly. If you has encountered this problem and solved it, please leave a message, thank you very muchProblem.png

ラベル(1)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,846件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

It is possible for you switch from S32DS for Power v1.2 to S32DS Power 2017.R1? 

We were facing similar issue for couple customers when Network connection was active - really slow IDE and build. But this issue was caused by some firewall settings on Customer side. You can try remove network cable and see if it helps. 

Jiri

0 件の賞賛
返信

1,846件の閲覧回数
建浩章
Contributor I

   Thanks for your reply. I tried the method you recommended, but it didn’t work. Anyway, thank you very much.

0 件の賞賛
返信